make: *** [Project_Settings/Startup_Code/__arm_end.o] Error 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

make: *** [Project_Settings/Startup_Code/__arm_end.o] Error 1

1,566件の閲覧回数
niranjanbc
Contributor IV

I was importing the project from codewarrior to KDS, when I do a build i am getting below error

make: *** [Project_Settings/Startup_Code/__arm_end.o] Error 1

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,364件の閲覧回数
kirantujare
Contributor IV

Hi Niranjan,
Did you solve the error?
If so, could you help me solve it?

0 件の賞賛
返信

1,364件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello niranjanbc,

About porting project from CodeWarrior to KDS, there are some attention,

please refer to here :

Importing MCU V10.6 projects (sample, using PE and MQX) under KDS

If still have any question , please contact us !

Hope it helps !

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信