Using MK20DX256xxx7 with KDS and KSDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using MK20DX256xxx7 with KDS and KSDK

跳至解决方案
86,176 次查看
stefdnt
Contributor I

Hello,

I am trying to create a Kinetis project with KDS, based on MK20DX256VLL7 (TWR-K20D72M).

I'd followed the steps described in the the KDS user Guide -> "Creating a Kinetis project".

When I reach the "Rapid Application Development" page, I am not able to select the SDK plugin.

If I select another chip (ex. MK60 or MK20DX256xxx10) it works good.

Is there a reason why the KSDK plugin could not be enabled with MK20DX256xxx7?

 

Regards.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,639 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello stephane,

I have checked KSDK1.3 and KSDK v2.0 , they don't support this chip now .

Sorry for the inconvenient to you . And I think you can use the Processor Expert to

development your project , it also easy to development .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,640 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello stephane,

I have checked KSDK1.3 and KSDK v2.0 , they don't support this chip now .

Sorry for the inconvenient to you . And I think you can use the Processor Expert to

development your project , it also easy to development .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复