MK24FN256xxx12 missing in processor selection while creating a new Kinetis project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK24FN256xxx12 missing in processor selection while creating a new Kinetis project

1,065 Views
rupeshgajurel
Contributor I


Hello, I need to include processor MK24FN256xxx12 for my project and I couldn't find it under the processors in devices. The only processor I was able to use was MK24Fn1M0xx12 but when I tried to load my code in internal flash, I get errors. However I was able to run the code if I download it in RAM. I assume this has to do with having different variant of the board.

How can I add MK24FN256xxx12 in the project?

Labels (1)
0 Kudos
Reply
1 Reply

1,011 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Rupesh,

Please refer to this thread to download and install the KSDK1.3 for MK24FN256xxx12:

Using Kinetis Design Studio v3.x with Kinetis SDK v2.0

pastedImage_2.png

then when you create project , you can see this option.

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply