Looking for "Resolve and export linked resources" checkbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for "Resolve and export linked resources" checkbox

Jump to solution
2,162 Views
robertpoor
Senior Contributor I

Erich Styger has given the solution to a problem that has been vexing me, except for one thing: his instructions indicate that you should check the "Resolve and export linked resources" checkbox when exporting the project, and he provides this graphic:

However, my version of KDS_v3 (Version: 3.2.0, with Eclipse Luna SR2 (4.4.2)), lacks that checkbox:

Screen Shot 2017-08-06 at 9.16.33 AM.png

I've recently applied updates.  What am I missing?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,668 Views
BlackNight
NXP Employee
NXP Employee

Hi Robert,

that additional checkbox is present with Eclipse Neon (MCUXpresso IDE) or Eclipse Oxygen (Breathing with Oxygen: DIY ARM Cortex-M C/C++ IDE and Toolchain with Eclipse Oxygen | MCU on Eclipse ). In previous Eclipse version (Luna, Kinetis Desing Studio) that option is not present, but it still will resolve the linked files.

pastedImage_1.png

So it will resolve them by default. With Neon or Oxygen you can disable it.

I hope this helps,

Erich

View solution in original post

1 Reply
1,669 Views
BlackNight
NXP Employee
NXP Employee

Hi Robert,

that additional checkbox is present with Eclipse Neon (MCUXpresso IDE) or Eclipse Oxygen (Breathing with Oxygen: DIY ARM Cortex-M C/C++ IDE and Toolchain with Eclipse Oxygen | MCU on Eclipse ). In previous Eclipse version (Luna, Kinetis Desing Studio) that option is not present, but it still will resolve the linked files.

pastedImage_1.png

So it will resolve them by default. With Neon or Oxygen you can disable it.

I hope this helps,

Erich