Looking for "Resolve and export linked resources" checkbox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Looking for "Resolve and export linked resources" checkbox

跳至解决方案
2,161 次查看
robertpoor
Senior Contributor I

Erich Styger has given the solution to a problem that has been vexing me, except for one thing: his instructions indicate that you should check the "Resolve and export linked resources" checkbox when exporting the project, and he provides this graphic:

However, my version of KDS_v3 (Version: 3.2.0, with Eclipse Luna SR2 (4.4.2)), lacks that checkbox:

Screen Shot 2017-08-06 at 9.16.33 AM.png

I've recently applied updates.  What am I missing?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,667 次查看
BlackNight
NXP Employee
NXP Employee

Hi Robert,

that additional checkbox is present with Eclipse Neon (MCUXpresso IDE) or Eclipse Oxygen (Breathing with Oxygen: DIY ARM Cortex-M C/C++ IDE and Toolchain with Eclipse Oxygen | MCU on Eclipse ). In previous Eclipse version (Luna, Kinetis Desing Studio) that option is not present, but it still will resolve the linked files.

pastedImage_1.png

So it will resolve them by default. With Neon or Oxygen you can disable it.

I hope this helps,

Erich

在原帖中查看解决方案

1 回复
1,668 次查看
BlackNight
NXP Employee
NXP Employee

Hi Robert,

that additional checkbox is present with Eclipse Neon (MCUXpresso IDE) or Eclipse Oxygen (Breathing with Oxygen: DIY ARM Cortex-M C/C++ IDE and Toolchain with Eclipse Oxygen | MCU on Eclipse ). In previous Eclipse version (Luna, Kinetis Desing Studio) that option is not present, but it still will resolve the linked files.

pastedImage_1.png

So it will resolve them by default. With Neon or Oxygen you can disable it.

I hope this helps,

Erich