Kinetis Design Studio KV4 Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio KV4 Support

ソリューションへジャンプ
1,809件の閲覧回数
michaelheidinge
Contributor III

Hi,

I'd like to use KDS for KV4 or KV5 series. When they will be supported?

-Michael

ラベル(1)
0 件の賞賛
返信
1 解決策
1,636件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

Yes, the latest version of KDS v3.2  now have the KV4 option when create project on menu.

We can also development KV5 series chip on  KDSv3.2, just need download KSDKv2.0 for the KV5x

chips, refer to this DOC:Using Kinetis Design Studio v3.x with Kinetis SDK v2.0 

Thus you can development on KDS. If you don't want to use the driver of KSDK, when you create project ,

just need select "Empty" on the Drivers:

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,636件の閲覧回数
michaelheidinge
Contributor III

Just noticed that KV4 is supported in th 3.2. release. All clear.

0 件の賞賛
返信
1,637件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

Yes, the latest version of KDS v3.2  now have the KV4 option when create project on menu.

We can also development KV5 series chip on  KDSv3.2, just need download KSDKv2.0 for the KV5x

chips, refer to this DOC:Using Kinetis Design Studio v3.x with Kinetis SDK v2.0 

Thus you can development on KDS. If you don't want to use the driver of KSDK, when you create project ,

just need select "Empty" on the Drivers:

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------