Kinetis Design Studio KV4 Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Design Studio KV4 Support

Jump to solution
1,806 Views
michaelheidinge
Contributor III

Hi,

I'd like to use KDS for KV4 or KV5 series. When they will be supported?

-Michael

Labels (1)
0 Kudos
Reply
1 Solution
1,633 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

Yes, the latest version of KDS v3.2  now have the KV4 option when create project on menu.

We can also development KV5 series chip on  KDSv3.2, just need download KSDKv2.0 for the KV5x

chips, refer to this DOC:Using Kinetis Design Studio v3.x with Kinetis SDK v2.0 

Thus you can development on KDS. If you don't want to use the driver of KSDK, when you create project ,

just need select "Empty" on the Drivers:

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,633 Views
michaelheidinge
Contributor III

Just noticed that KV4 is supported in th 3.2. release. All clear.

0 Kudos
Reply
1,634 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

Yes, the latest version of KDS v3.2  now have the KV4 option when create project on menu.

We can also development KV5 series chip on  KDSv3.2, just need download KSDKv2.0 for the KV5x

chips, refer to this DOC:Using Kinetis Design Studio v3.x with Kinetis SDK v2.0 

Thus you can development on KDS. If you don't want to use the driver of KSDK, when you create project ,

just need select "Empty" on the Drivers:

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------