KDS linker error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS linker error

Jump to solution
2,960 Views
hunt
Contributor II

Good morning,

For the last days I am struggling with a problem with KDS.

 

I developed a C-Project for the FRDM-k64f board, using KDS and Processor Expert (I started a KDS project).

Now I need to add a C++ class to my project.

 

In order to do so, I renamed the main.c to main.cpp, and added the include directive as following:

19065_19065.gif1.gif

 

but I have a problem:

The compiling of the files is successful, but the linker gives error to some functions (I think for the linking file order).

 

Is someone able to help me?

Thank you in advance.

 

09:45:27 **** Build of configuration Debug for project Freescale_chrono ****

make all

'Building file: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/CPU_Init.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Static_Code/System/CPU_Init.d" -MT"Static_Code/System/CPU_Init.o" -c -o "Static_Code/System/CPU_Init.o" "C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/CPU_Init.c"

'Finished building: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/CPU_Init.c'

' '

'Building file: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/Peripherals_Init.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Static_Code/System/Peripherals_Init.d" -MT"Static_Code/System/Peripherals_Init.o" -c -o "Static_Code/System/Peripherals_Init.o" "C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/Peripherals_Init.c"

'Finished building: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/Peripherals_Init.c'

' '

'Building file: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/Vectors.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Static_Code/System/Vectors.d" -MT"Static_Code/System/Vectors.o" -c -o "Static_Code/System/Vectors.o" "C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/Vectors.c"

'Finished building: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system/Vectors.c'

' '

'Building file: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals/LPTMR0_Init.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Static_Code/Peripherals/LPTMR0_Init.d" -MT"Static_Code/Peripherals/LPTMR0_Init.o" -c -o "Static_Code/Peripherals/LPTMR0_Init.o" "C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals/LPTMR0_Init.c"

'Finished building: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals/LPTMR0_Init.c'

' '

'Building file: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals/USB0_Init.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Static_Code/Peripherals/USB0_Init.d" -MT"Static_Code/Peripherals/USB0_Init.o" -c -o "Static_Code/Peripherals/USB0_Init.o" "C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals/USB0_Init.c"

'Finished building: C:/Freescale/KDS_1.1.1/eclipse/ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals/USB0_Init.c'

' '

'Building file: ../Sources/LCD/UTFT.cpp'

'Invoking: Cross ARM C++ Compiler'

arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=gnu++11 -fabi-version=0 -MMD -MP -MF"Sources/LCD/UTFT.d" -MT"Sources/LCD/UTFT.o" -c -o "Sources/LCD/UTFT.o" "../Sources/LCD/UTFT.cpp"

In file included from ../Sources/LCD/UTFT.h:165:0,

                 from ../Sources/LCD/UTFT.cpp:38:

../Sources/LCD/hardware/HW_FRDM_defines.h:28:0: warning: "regtype" redefined [enabled by default]

#define regtype volatile uint32_t

^

In file included from ../Sources/LCD/UTFT.cpp:38:0:

../Sources/LCD/UTFT.h:160:0: note: this is the location of the previous definition

#define regtype volatile uint8_t

^

In file included from ../Sources/LCD/UTFT.h:165:0,

                 from ../Sources/LCD/UTFT.cpp:38:

../Sources/LCD/hardware/HW_FRDM_defines.h:29:0: warning: "regsize" redefined [enabled by default]

#define regsize uint32_t

^

In file included from ../Sources/LCD/UTFT.cpp:38:0:

../Sources/LCD/UTFT.h:161:0: note: this is the location of the previous definition

#define regsize uint8_t

^

In file included from ../Sources/LCD/UTFT.h:165:0,

                 from ../Sources/LCD/UTFT.cpp:38:

../Sources/LCD/hardware/HW_FRDM_defines.h:30:0: warning: "bitmapdatatype" redefined [enabled by default]

#define bitmapdatatype unsigned short*

^

In file included from ../Sources/LCD/UTFT.cpp:38:0:

../Sources/LCD/UTFT.h:159:0: note: this is the location of the previous definition

#define bitmapdatatype unsigned int*

^

'Finished building: ../Sources/LCD/UTFT.cpp'

' '

'Building file: ../Sources/BT_serial.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/BT_serial.d" -MT"Sources/BT_serial.o" -c -o "Sources/BT_serial.o" "../Sources/BT_serial.c"

'Finished building: ../Sources/BT_serial.c'

' '

'Building file: ../Sources/Battery.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/Battery.d" -MT"Sources/Battery.o" -c -o "Sources/Battery.o" "../Sources/Battery.c"

'Finished building: ../Sources/Battery.c'

' '

'Building file: ../Sources/Chrono.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/Chrono.d" -MT"Sources/Chrono.o" -c -o "Sources/Chrono.o" "../Sources/Chrono.c"

'Finished building: ../Sources/Chrono.c'

' '

'Building file: ../Sources/CommandHandler.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/CommandHandler.d" -MT"Sources/CommandHandler.o" -c -o "Sources/CommandHandler.o" "../Sources/CommandHandler.c"

'Finished building: ../Sources/CommandHandler.c'

' '

'Building file: ../Sources/Events.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/Events.d" -MT"Sources/Events.o" -c -o "Sources/Events.o" "../Sources/Events.c"

'Finished building: ../Sources/Events.c'

' '

'Building file: ../Sources/RTC.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/RTC.d" -MT"Sources/RTC.o" -c -o "Sources/RTC.o" "../Sources/RTC.c"

'Finished building: ../Sources/RTC.c'

' '

'Building file: ../Sources/Serial.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/Serial.d" -MT"Sources/Serial.o" -c -o "Sources/Serial.o" "../Sources/Serial.c"

'Finished building: ../Sources/Serial.c'

' '

'Building file: ../Sources/USB_serial.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/USB_serial.d" -MT"Sources/USB_serial.o" -c -o "Sources/USB_serial.o" "../Sources/USB_serial.c"

'Finished building: ../Sources/USB_serial.c'

' '

'Building file: ../Sources/UTIL64b.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Sources/UTIL64b.d" -MT"Sources/UTIL64b.o" -c -o "Sources/UTIL64b.o" "../Sources/UTIL64b.c"

'Finished building: ../Sources/UTIL64b.c'

' '

'Building file: ../Sources/main.cpp'

'Invoking: Cross ARM C++ Compiler'

arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=gnu++11 -fabi-version=0 -MMD -MP -MF"Sources/main.d" -MT"Sources/main.o" -c -o "Sources/main.o" "../Sources/main.cpp"

'Finished building: ../Sources/main.cpp'

' '

'Building file: ../Project_Settings/Startup_Code/startup.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Project_Settings/Startup_Code/startup.d" -MT"Project_Settings/Startup_Code/startup.o" -c -o "Project_Settings/Startup_Code/startup.o" "../Project_Settings/Startup_Code/startup.c"

'Finished building: ../Project_Settings/Startup_Code/startup.c'

' '

'Building file: ../Generated_Code/AD1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/AD1.d" -MT"Generated_Code/AD1.o" -c -o "Generated_Code/AD1.o" "../Generated_Code/AD1.c"

'Finished building: ../Generated_Code/AD1.c'

' '

'Building file: ../Generated_Code/ASerialLdd1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/ASerialLdd1.d" -MT"Generated_Code/ASerialLdd1.o" -c -o "Generated_Code/ASerialLdd1.o" "../Generated_Code/ASerialLdd1.c"

'Finished building: ../Generated_Code/ASerialLdd1.c'

' '

'Building file: ../Generated_Code/BT1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/BT1.d" -MT"Generated_Code/BT1.o" -c -o "Generated_Code/BT1.o" "../Generated_Code/BT1.c"

'Finished building: ../Generated_Code/BT1.c'

' '

'Building file: ../Generated_Code/BUZZER.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/BUZZER.d" -MT"Generated_Code/BUZZER.o" -c -o "Generated_Code/BUZZER.o" "../Generated_Code/BUZZER.c"

'Finished building: ../Generated_Code/BUZZER.c'

' '

'Building file: ../Generated_Code/BUZZERTIMEOUT.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/BUZZERTIMEOUT.d" -MT"Generated_Code/BUZZERTIMEOUT.o" -c -o "Generated_Code/BUZZERTIMEOUT.o" "../Generated_Code/BUZZERTIMEOUT.c"

'Finished building: ../Generated_Code/BUZZERTIMEOUT.c'

' '

'Building file: ../Generated_Code/CDC1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/CDC1.d" -MT"Generated_Code/CDC1.o" -c -o "Generated_Code/CDC1.o" "../Generated_Code/CDC1.c"

'Finished building: ../Generated_Code/CDC1.c'

' '

'Building file: ../Generated_Code/CS1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/CS1.d" -MT"Generated_Code/CS1.o" -c -o "Generated_Code/CS1.o" "../Generated_Code/CS1.c"

'Finished building: ../Generated_Code/CS1.c'

' '

'Building file: ../Generated_Code/Cpu.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/Cpu.d" -MT"Generated_Code/Cpu.o" -c -o "Generated_Code/Cpu.o" "../Generated_Code/Cpu.c"

'Finished building: ../Generated_Code/Cpu.c'

' '

'Building file: ../Generated_Code/FLASH1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/FLASH1.d" -MT"Generated_Code/FLASH1.o" -c -o "Generated_Code/FLASH1.o" "../Generated_Code/FLASH1.c"

'Finished building: ../Generated_Code/FLASH1.c'

' '

'Building file: ../Generated_Code/LCD_CS.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_CS.d" -MT"Generated_Code/LCD_CS.o" -c -o "Generated_Code/LCD_CS.o" "../Generated_Code/LCD_CS.c"

'Finished building: ../Generated_Code/LCD_CS.c'

' '

'Building file: ../Generated_Code/LCD_DB0.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB0.d" -MT"Generated_Code/LCD_DB0.o" -c -o "Generated_Code/LCD_DB0.o" "../Generated_Code/LCD_DB0.c"

'Finished building: ../Generated_Code/LCD_DB0.c'

' '

'Building file: ../Generated_Code/LCD_DB1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB1.d" -MT"Generated_Code/LCD_DB1.o" -c -o "Generated_Code/LCD_DB1.o" "../Generated_Code/LCD_DB1.c"

'Finished building: ../Generated_Code/LCD_DB1.c'

' '

'Building file: ../Generated_Code/LCD_DB10.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB10.d" -MT"Generated_Code/LCD_DB10.o" -c -o "Generated_Code/LCD_DB10.o" "../Generated_Code/LCD_DB10.c"

'Finished building: ../Generated_Code/LCD_DB10.c'

' '

'Building file: ../Generated_Code/LCD_DB11.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB11.d" -MT"Generated_Code/LCD_DB11.o" -c -o "Generated_Code/LCD_DB11.o" "../Generated_Code/LCD_DB11.c"

'Finished building: ../Generated_Code/LCD_DB11.c'

' '

'Building file: ../Generated_Code/LCD_DB12.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB12.d" -MT"Generated_Code/LCD_DB12.o" -c -o "Generated_Code/LCD_DB12.o" "../Generated_Code/LCD_DB12.c"

'Finished building: ../Generated_Code/LCD_DB12.c'

' '

'Building file: ../Generated_Code/LCD_DB13.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB13.d" -MT"Generated_Code/LCD_DB13.o" -c -o "Generated_Code/LCD_DB13.o" "../Generated_Code/LCD_DB13.c"

'Finished building: ../Generated_Code/LCD_DB13.c'

' '

'Building file: ../Generated_Code/LCD_DB14.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB14.d" -MT"Generated_Code/LCD_DB14.o" -c -o "Generated_Code/LCD_DB14.o" "../Generated_Code/LCD_DB14.c"

'Finished building: ../Generated_Code/LCD_DB14.c'

' '

'Building file: ../Generated_Code/LCD_DB15.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB15.d" -MT"Generated_Code/LCD_DB15.o" -c -o "Generated_Code/LCD_DB15.o" "../Generated_Code/LCD_DB15.c"

'Finished building: ../Generated_Code/LCD_DB15.c'

' '

'Building file: ../Generated_Code/LCD_DB2.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB2.d" -MT"Generated_Code/LCD_DB2.o" -c -o "Generated_Code/LCD_DB2.o" "../Generated_Code/LCD_DB2.c"

'Finished building: ../Generated_Code/LCD_DB2.c'

' '

'Building file: ../Generated_Code/LCD_DB3.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB3.d" -MT"Generated_Code/LCD_DB3.o" -c -o "Generated_Code/LCD_DB3.o" "../Generated_Code/LCD_DB3.c"

'Finished building: ../Generated_Code/LCD_DB3.c'

' '

'Building file: ../Generated_Code/LCD_DB4.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB4.d" -MT"Generated_Code/LCD_DB4.o" -c -o "Generated_Code/LCD_DB4.o" "../Generated_Code/LCD_DB4.c"

'Finished building: ../Generated_Code/LCD_DB4.c'

' '

'Building file: ../Generated_Code/LCD_DB5.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB5.d" -MT"Generated_Code/LCD_DB5.o" -c -o "Generated_Code/LCD_DB5.o" "../Generated_Code/LCD_DB5.c"

'Finished building: ../Generated_Code/LCD_DB5.c'

' '

'Building file: ../Generated_Code/LCD_DB6.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB6.d" -MT"Generated_Code/LCD_DB6.o" -c -o "Generated_Code/LCD_DB6.o" "../Generated_Code/LCD_DB6.c"

'Finished building: ../Generated_Code/LCD_DB6.c'

' '

'Building file: ../Generated_Code/LCD_DB7.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB7.d" -MT"Generated_Code/LCD_DB7.o" -c -o "Generated_Code/LCD_DB7.o" "../Generated_Code/LCD_DB7.c"

'Finished building: ../Generated_Code/LCD_DB7.c'

' '

'Building file: ../Generated_Code/LCD_DB8.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB8.d" -MT"Generated_Code/LCD_DB8.o" -c -o "Generated_Code/LCD_DB8.o" "../Generated_Code/LCD_DB8.c"

'Finished building: ../Generated_Code/LCD_DB8.c'

' '

'Building file: ../Generated_Code/LCD_DB9.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_DB9.d" -MT"Generated_Code/LCD_DB9.o" -c -o "Generated_Code/LCD_DB9.o" "../Generated_Code/LCD_DB9.c"

'Finished building: ../Generated_Code/LCD_DB9.c'

' '

'Building file: ../Generated_Code/LCD_LEDA.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_LEDA.d" -MT"Generated_Code/LCD_LEDA.o" -c -o "Generated_Code/LCD_LEDA.o" "../Generated_Code/LCD_LEDA.c"

'Finished building: ../Generated_Code/LCD_LEDA.c'

' '

'Building file: ../Generated_Code/LCD_RS.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_RS.d" -MT"Generated_Code/LCD_RS.o" -c -o "Generated_Code/LCD_RS.o" "../Generated_Code/LCD_RS.c"

'Finished building: ../Generated_Code/LCD_RS.c'

' '

'Building file: ../Generated_Code/LCD_RST.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_RST.d" -MT"Generated_Code/LCD_RST.o" -c -o "Generated_Code/LCD_RST.o" "../Generated_Code/LCD_RST.c"

'Finished building: ../Generated_Code/LCD_RST.c'

' '

'Building file: ../Generated_Code/LCD_WR.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LCD_WR.d" -MT"Generated_Code/LCD_WR.o" -c -o "Generated_Code/LCD_WR.o" "../Generated_Code/LCD_WR.c"

'Finished building: ../Generated_Code/LCD_WR.c'

' '

'Building file: ../Generated_Code/LED_B.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LED_B.d" -MT"Generated_Code/LED_B.o" -c -o "Generated_Code/LED_B.o" "../Generated_Code/LED_B.c"

'Finished building: ../Generated_Code/LED_B.c'

' '

'Building file: ../Generated_Code/LED_G.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LED_G.d" -MT"Generated_Code/LED_G.o" -c -o "Generated_Code/LED_G.o" "../Generated_Code/LED_G.c"

'Finished building: ../Generated_Code/LED_G.c'

' '

'Building file: ../Generated_Code/LED_R.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/LED_R.d" -MT"Generated_Code/LED_R.o" -c -o "Generated_Code/LED_R.o" "../Generated_Code/LED_R.c"

'Finished building: ../Generated_Code/LED_R.c'

' '

'Building file: ../Generated_Code/PE_LDD.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/PE_LDD.d" -MT"Generated_Code/PE_LDD.o" -c -o "Generated_Code/PE_LDD.o" "../Generated_Code/PE_LDD.c"

'Finished building: ../Generated_Code/PE_LDD.c'

' '

'Building file: ../Generated_Code/PhotoInt.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/PhotoInt.d" -MT"Generated_Code/PhotoInt.o" -c -o "Generated_Code/PhotoInt.o" "../Generated_Code/PhotoInt.c"

'Finished building: ../Generated_Code/PhotoInt.c'

' '

'Building file: ../Generated_Code/Pins1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/Pins1.d" -MT"Generated_Code/Pins1.o" -c -o "Generated_Code/Pins1.o" "../Generated_Code/Pins1.c"

'Finished building: ../Generated_Code/Pins1.c'

' '

'Building file: ../Generated_Code/Rx1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/Rx1.d" -MT"Generated_Code/Rx1.o" -c -o "Generated_Code/Rx1.o" "../Generated_Code/Rx1.c"

'Finished building: ../Generated_Code/Rx1.c'

' '

'Building file: ../Generated_Code/SPI0.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/SPI0.d" -MT"Generated_Code/SPI0.o" -c -o "Generated_Code/SPI0.o" "../Generated_Code/SPI0.c"

'Finished building: ../Generated_Code/SPI0.c'

' '

'Building file: ../Generated_Code/STRIP_LED_B.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/STRIP_LED_B.d" -MT"Generated_Code/STRIP_LED_B.o" -c -o "Generated_Code/STRIP_LED_B.o" "../Generated_Code/STRIP_LED_B.c"

'Finished building: ../Generated_Code/STRIP_LED_B.c'

' '

'Building file: ../Generated_Code/STRIP_LED_G.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/STRIP_LED_G.d" -MT"Generated_Code/STRIP_LED_G.o" -c -o "Generated_Code/STRIP_LED_G.o" "../Generated_Code/STRIP_LED_G.c"

'Finished building: ../Generated_Code/STRIP_LED_G.c'

' '

'Building file: ../Generated_Code/STRIP_LED_R.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/STRIP_LED_R.d" -MT"Generated_Code/STRIP_LED_R.o" -c -o "Generated_Code/STRIP_LED_R.o" "../Generated_Code/STRIP_LED_R.c"

'Finished building: ../Generated_Code/STRIP_LED_R.c'

' '

'Building file: ../Generated_Code/STRIP_LED_R_TIMEOUT.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/STRIP_LED_R_TIMEOUT.d" -MT"Generated_Code/STRIP_LED_R_TIMEOUT.o" -c -o "Generated_Code/STRIP_LED_R_TIMEOUT.o" "../Generated_Code/STRIP_LED_R_TIMEOUT.c"

'Finished building: ../Generated_Code/STRIP_LED_R_TIMEOUT.c'

' '

'Building file: ../Generated_Code/Serial1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/Serial1.d" -MT"Generated_Code/Serial1.o" -c -o "Generated_Code/Serial1.o" "../Generated_Code/Serial1.c"

'Finished building: ../Generated_Code/Serial1.c'

' '

'Building file: ../Generated_Code/Tx1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/Tx1.d" -MT"Generated_Code/Tx1.o" -c -o "Generated_Code/Tx1.o" "../Generated_Code/Tx1.c"

'Finished building: ../Generated_Code/Tx1.c'

' '

'Building file: ../Generated_Code/USB1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/USB1.d" -MT"Generated_Code/USB1.o" -c -o "Generated_Code/USB1.o" "../Generated_Code/USB1.c"

'Finished building: ../Generated_Code/USB1.c'

' '

'Building file: ../Generated_Code/UTIL1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/UTIL1.d" -MT"Generated_Code/UTIL1.o" -c -o "Generated_Code/UTIL1.o" "../Generated_Code/UTIL1.c"

'Finished building: ../Generated_Code/UTIL1.c'

' '

'Building file: ../Generated_Code/WAIT1.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/WAIT1.d" -MT"Generated_Code/WAIT1.o" -c -o "Generated_Code/WAIT1.o" "../Generated_Code/WAIT1.c"

'Finished building: ../Generated_Code/WAIT1.c'

' '

'Building file: ../Generated_Code/usb_cdc.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_cdc.d" -MT"Generated_Code/usb_cdc.o" -c -o "Generated_Code/usb_cdc.o" "../Generated_Code/usb_cdc.c"

'Finished building: ../Generated_Code/usb_cdc.c'

' '

'Building file: ../Generated_Code/usb_cdc_pstn.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_cdc_pstn.d" -MT"Generated_Code/usb_cdc_pstn.o" -c -o "Generated_Code/usb_cdc_pstn.o" "../Generated_Code/usb_cdc_pstn.c"

'Finished building: ../Generated_Code/usb_cdc_pstn.c'

' '

'Building file: ../Generated_Code/usb_class.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_class.d" -MT"Generated_Code/usb_class.o" -c -o "Generated_Code/usb_class.o" "../Generated_Code/usb_class.c"

'Finished building: ../Generated_Code/usb_class.c'

' '

'Building file: ../Generated_Code/usb_dci_kinetis.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_dci_kinetis.d" -MT"Generated_Code/usb_dci_kinetis.o" -c -o "Generated_Code/usb_dci_kinetis.o" "../Generated_Code/usb_dci_kinetis.c"

'Finished building: ../Generated_Code/usb_dci_kinetis.c'

' '

'Building file: ../Generated_Code/usb_descriptor.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_descriptor.d" -MT"Generated_Code/usb_descriptor.o" -c -o "Generated_Code/usb_descriptor.o" "../Generated_Code/usb_descriptor.c"

'Finished building: ../Generated_Code/usb_descriptor.c'

' '

'Building file: ../Generated_Code/usb_driver.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_driver.d" -MT"Generated_Code/usb_driver.o" -c -o "Generated_Code/usb_driver.o" "../Generated_Code/usb_driver.c"

'Finished building: ../Generated_Code/usb_driver.c'

' '

'Building file: ../Generated_Code/usb_framework.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/usb_framework.d" -MT"Generated_Code/usb_framework.o" -c -o "Generated_Code/usb_framework.o" "../Generated_Code/usb_framework.c"

'Finished building: ../Generated_Code/usb_framework.c'

' '

'Building file: ../Generated_Code/wdt_kinetis.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/system" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/iofiles" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Sources" -I"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Generated_Code" -I"C:\Freescale\KDS_1.1.1\eclipse\ProcessorExpert/lib/Kinetis/pdd2/MK64FN1M0LQ12/peripherals" -std=c99 -MMD -MP -MF"Generated_Code/wdt_kinetis.d" -MT"Generated_Code/wdt_kinetis.o" -c -o "Generated_Code/wdt_kinetis.o" "../Generated_Code/wdt_kinetis.c"

'Finished building: ../Generated_Code/wdt_kinetis.c'

' '

'Building target: Freescale_chrono.elf'

'Invoking: Cross ARM C++ Linker'

arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -T "C:/Users/Toshiba/workspace_kds/Freescale_chrono/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"C:/Users/Toshiba/workspace_kds/Freescale_chrono/Project_Settings/Linker_Files" -Wl,-Map,"Freescale_chrono.map" -nanolibc -o "Freescale_chrono.elf"  ./Static_Code/System/CPU_Init.o ./Static_Code/System/Peripherals_Init.o ./Static_Code/System/Vectors.o  ./Static_Code/Peripherals/LPTMR0_Init.o ./Static_Code/Peripherals/USB0_Init.o  ./Sources/LCD/UTFT.o  ./Sources/BT_serial.o ./Sources/Battery.o ./Sources/Chrono.o ./Sources/CommandHandler.o ./Sources/Events.o ./Sources/RTC.o ./Sources/Serial.o ./Sources/USB_serial.o ./Sources/UTIL64b.o ./Sources/main.o  ./Project_Settings/Startup_Code/startup.o  ./Generated_Code/AD1.o ./Generated_Code/ASerialLdd1.o ./Generated_Code/BT1.o ./Generated_Code/BUZZER.o ./Generated_Code/BUZZERTIMEOUT.o ./Generated_Code/CDC1.o ./Generated_Code/CS1.o ./Generated_Code/Cpu.o ./Generated_Code/FLASH1.o ./Generated_Code/LCD_CS.o ./Generated_Code/LCD_DB0.o ./Generated_Code/LCD_DB1.o ./Generated_Code/LCD_DB10.o ./Generated_Code/LCD_DB11.o ./Generated_Code/LCD_DB12.o ./Generated_Code/LCD_DB13.o ./Generated_Code/LCD_DB14.o ./Generated_Code/LCD_DB15.o ./Generated_Code/LCD_DB2.o ./Generated_Code/LCD_DB3.o ./Generated_Code/LCD_DB4.o ./Generated_Code/LCD_DB5.o ./Generated_Code/LCD_DB6.o ./Generated_Code/LCD_DB7.o ./Generated_Code/LCD_DB8.o ./Generated_Code/LCD_DB9.o ./Generated_Code/LCD_LEDA.o ./Generated_Code/LCD_RS.o ./Generated_Code/LCD_RST.o ./Generated_Code/LCD_WR.o ./Generated_Code/LED_B.o ./Generated_Code/LED_G.o ./Generated_Code/LED_R.o ./Generated_Code/PE_LDD.o ./Generated_Code/PhotoInt.o ./Generated_Code/Pins1.o ./Generated_Code/Rx1.o ./Generated_Code/SPI0.o ./Generated_Code/STRIP_LED_B.o ./Generated_Code/STRIP_LED_G.o ./Generated_Code/STRIP_LED_R.o ./Generated_Code/STRIP_LED_R_TIMEOUT.o ./Generated_Code/Serial1.o ./Generated_Code/Tx1.o ./Generated_Code/USB1.o ./Generated_Code/UTIL1.o ./Generated_Code/WAIT1.o ./Generated_Code/usb_cdc.o ./Generated_Code/usb_cdc_pstn.o ./Generated_Code/usb_class.o ./Generated_Code/usb_dci_kinetis.o ./Generated_Code/usb_descriptor.o ./Generated_Code/usb_driver.o ./Generated_Code/usb_framework.o ./Generated_Code/wdt_kinetis.o 

./Sources/main.o: In function `main':

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:157: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:159: undefined reference to `CDC1_App_Task(unsigned char*, unsigned int)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:162: undefined reference to `CDC1_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:167: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:169: undefined reference to `CDC1_App_Task(unsigned char*, unsigned int)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:172: undefined reference to `CDC1_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:177: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:179: undefined reference to `CDC1_App_Task(unsigned char*, unsigned int)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:182: undefined reference to `CDC1_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:222: undefined reference to `USB_ceck_command(char*, unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:224: undefined reference to `BT_ceck_command(char*, unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:238: undefined reference to `USB_sendStart()'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:244: undefined reference to `BT_sendStart()'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:285: undefined reference to `USB_sendTimeLap(unsigned int, unsigned long long*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:291: undefined reference to `BT_sendTimeLap(unsigned int, unsigned long long*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:305: undefined reference to `USB_sendTimeLap(unsigned int, unsigned long long*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:311: undefined reference to `BT_sendTimeLap(unsigned int, unsigned long long*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:336: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:349: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:353: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:355: undefined reference to `CDC1_App_Task(unsigned char*, unsigned int)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:358: undefined reference to `CDC1_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:366: undefined reference to `Battery_check(unsigned short*, unsigned int)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:369: undefined reference to `BT_SendString(unsigned char*)'

C:\Users\Toshiba\workspace_kds\Freescale_chrono\Debug/../Sources/main.cpp:375: undefined reference to `SendBatteryData(unsigned short*)'

collect2.exe: error: ld returned 1 exit status

make: *** [Freescale_chrono.elf] Error 1

 

 

09:46:55 Build Finished (took 1m:27s.136ms)

Labels (1)
Tags (3)
1 Solution
2,613 Views
hunt
Contributor II

I solved my Issue.

If someone has the same problem, the solution is to use the extern "C" directive for the C functions used inside the .cpp file. Otherwise the linker (not the compiler), will give you the error.


Thank you anyway.

View solution in original post

2 Replies
2,614 Views
hunt
Contributor II

I solved my Issue.

If someone has the same problem, the solution is to use the extern "C" directive for the C functions used inside the .cpp file. Otherwise the linker (not the compiler), will give you the error.


Thank you anyway.

2,613 Views
DavidS
NXP Employee
NXP Employee

Thank you for sharing your solution.

Regards,

David

0 Kudos
Reply