P3S0210BQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3S0210BQ

Jump to solution
5,758 Views
JaeHwan
Contributor II

Hi.

I don't know why output voltage drop(VCCP1 & VCCP2 Output voltage : 1.65V).

Using voltage is below.

VCCR : 3.58V

VCCS : 3.3V

VCCE : 3.3V

VCCP1, VCCP2 : 3.3V

 

1-host : 2-device

host is stm32(Only normal I2C, not I3C)

device is normal eeproms

 

 

 

Thank you.

캡처.JPG

0 Kudos
Reply
1 Solution
5,344 Views
JaeHwan
Contributor II

Hi. guoweisun!

 

I solved.

Add 47pF capacitor at Input and output lines.

 

Thank you.

View solution in original post

0 Kudos
Reply
14 Replies
5,753 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Could you please help and share with your schematic?

 

0 Kudos
Reply
5,753 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Could you please help and share with your schematic?

 

0 Kudos
Reply
5,749 Views
JaeHwan
Contributor II

Hi. guoweisun!

 

Thank you for your fast answer!

캡처1.JPG

1-host(stm32) has above pull-up value.

 

캡처.JPG

 

0 Kudos
Reply
5,734 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the IIC use case you should add the pull up resistors.

guoweisun_0-1753322115879.png

 

0 Kudos
Reply
5,722 Views
JaeHwan
Contributor II

Hi. guoweisun!

Thank you for your fast answer!

 

1-host have Pull-up.

 

캡처.JPG

0 Kudos
Reply
5,720 Views
guoweisun
NXP TechSupport
NXP TechSupport

On both sides need pull up resistors.

Did you add on both sides?

0 Kudos
Reply
5,680 Views
JaeHwan
Contributor II
Hi, guoweisun!

Yes. add on both sides!

above schematics.
0 Kudos
Reply
5,565 Views
guoweisun
NXP TechSupport
NXP TechSupport

 For the output voltage drop waveform,can you give clear picture again for better analysis?

0 Kudos
Reply
5,555 Views
JaeHwan
Contributor II

Hi.

 

캡처.JPG

 

캡처1.JPG

Thank you.

0 Kudos
Reply
5,551 Views
guoweisun
NXP TechSupport
NXP TechSupport

Can you zoom in your waveform? I need to see the  drop value.

0 Kudos
Reply
5,545 Views
JaeHwan
Contributor II

20250723_063325.jpg

0 Kudos
Reply
5,536 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

The input signal is not up to 3.3V.,can you test the input signal disconnect with this P3S0210BQ to confirm whether it's 3.3V signal?

0 Kudos
Reply
5,534 Views
JaeHwan
Contributor II

캡처.JPG

0 Kudos
Reply
5,345 Views
JaeHwan
Contributor II

Hi. guoweisun!

 

I solved.

Add 47pF capacitor at Input and output lines.

 

Thank you.

0 Kudos
Reply