My Win10 can not install FreeMaster3.1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

My Win10 can not install FreeMaster3.1.2

Jump to solution
4,691 Views
ArchieLuo
Contributor III

捕获.PNG

 

屏幕截图 2021-07-29 112335.png

 Why?Can you help me? Thanks!

 

0 Kudos
Reply
1 Solution
4,681 Views
iulian_stan
NXP Employee
NXP Employee

Hi,

According to your installation log the installer was unable to clear previous version of FreeMASTER 3.1. It's hard to say what exactly caused the failure. Here are a few options to try:

  • Could you uninstall previous FreeMASTER 3.1 from "Program and Features" or by running "FreeMASTER 3.1\_FreeMASTER_installation\Uninstall FreeMASTER.exe"
  • In case there's no such entry in "Program and Features" or the uninstaller is missing - remove "FreeMASTER 3.1" folder and all its content manually.
    Try launching the installer.
  • If it complains about a previous installation you may need to remove FreeMASTER 3.1 registry entry from "C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml" - a quick solution is to rename original file to ".com.zerog.registry_backup.xm" in case there other entries beside FreeMASTER.

Hope this helps.

View solution in original post

0 Kudos
Reply
3 Replies
4,682 Views
iulian_stan
NXP Employee
NXP Employee

Hi,

According to your installation log the installer was unable to clear previous version of FreeMASTER 3.1. It's hard to say what exactly caused the failure. Here are a few options to try:

  • Could you uninstall previous FreeMASTER 3.1 from "Program and Features" or by running "FreeMASTER 3.1\_FreeMASTER_installation\Uninstall FreeMASTER.exe"
  • In case there's no such entry in "Program and Features" or the uninstaller is missing - remove "FreeMASTER 3.1" folder and all its content manually.
    Try launching the installer.
  • If it complains about a previous installation you may need to remove FreeMASTER 3.1 registry entry from "C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml" - a quick solution is to rename original file to ".com.zerog.registry_backup.xm" in case there other entries beside FreeMASTER.

Hope this helps.

0 Kudos
Reply
4,033 Views
1111
Contributor I

安装好之后为什么不用输入激活码?不用输入激活码可以用吗?

 

0 Kudos
Reply
4,666 Views
ArchieLuo
Contributor III

Thanks!

"remove "FreeMASTER 3.1" folder and all its content manually".

0 Kudos
Reply