My Win10 can not install FreeMaster3.1.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

My Win10 can not install FreeMaster3.1.2

跳至解决方案
3,520 次查看
ArchieLuo
Contributor III

捕获.PNG

屏幕截图 2021-07-29 112335.png

 Why?Can you help me? Thanks!

0 项奖励
回复
1 解答
3,510 次查看
iulian_stan
NXP Employee
NXP Employee

Hi,

According to your installation log the installer was unable to clear previous version of FreeMASTER 3.1. It's hard to say what exactly caused the failure. Here are a few options to try:

  • Could you uninstall previous FreeMASTER 3.1 from "Program and Features" or by running "FreeMASTER 3.1\_FreeMASTER_installation\Uninstall FreeMASTER.exe"
  • In case there's no such entry in "Program and Features" or the uninstaller is missing - remove "FreeMASTER 3.1" folder and all its content manually.
    Try launching the installer.
  • If it complains about a previous installation you may need to remove FreeMASTER 3.1 registry entry from "C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml" - a quick solution is to rename original file to ".com.zerog.registry_backup.xm" in case there other entries beside FreeMASTER.

Hope this helps.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,511 次查看
iulian_stan
NXP Employee
NXP Employee

Hi,

According to your installation log the installer was unable to clear previous version of FreeMASTER 3.1. It's hard to say what exactly caused the failure. Here are a few options to try:

  • Could you uninstall previous FreeMASTER 3.1 from "Program and Features" or by running "FreeMASTER 3.1\_FreeMASTER_installation\Uninstall FreeMASTER.exe"
  • In case there's no such entry in "Program and Features" or the uninstaller is missing - remove "FreeMASTER 3.1" folder and all its content manually.
    Try launching the installer.
  • If it complains about a previous installation you may need to remove FreeMASTER 3.1 registry entry from "C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml" - a quick solution is to rename original file to ".com.zerog.registry_backup.xm" in case there other entries beside FreeMASTER.

Hope this helps.

0 项奖励
回复
2,862 次查看
1111
Contributor I

安装好之后为什么不用输入激活码?不用输入激活码可以用吗?

 

0 项奖励
回复
3,495 次查看
ArchieLuo
Contributor III

Thanks!

"remove "FreeMASTER 3.1" folder and all its content manually".

0 项奖励
回复