FRDM Training Hub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM Training Hub

FRDM Training Hub


Restricted Beta Program

  • Comprehensive software and tools for seamless prototyping and rapid development
  • Scale your project with modular, quick-start FRDM and expansion boards
  • Leverage our application code hub or GoPoint to access 180+ code snippets and demos

  • Leverage FRDM Training Hub to learn from the experts
  • Not sure where to start ?

ディスカッション

ソート順:
Whether you're a student, hobbyist, or professional developer, the FRDM Development Platform by NXP is your gateway to building powerful embedded applications—quickly and affordably. In this beginner-friendly guide, you’ll learn: What FRDM boards are and how they compare to other NXP evaluation kits Who the platform is designed for How to buy and get started with your first board What’s new in the latest FRDM series featuring MCX microcontrollers and i.MX processors How the FRDM ecosystem supports your development with modular hardware, software tools, and ready-to-use code examples
記事全体を表示
FRDM Training and Resources This article provide a guide of available resources for FRDM Development boards to help you to find and use available resources (Boards, Guides, Hands-On Trainings and more)
記事全体を表示
This article mainly introduces the design of the FRDM-MCXE31B and how to import and run ACH examples. Through this article, readers can gain a detailed understanding of the main resources of the FRDM-MCXE31B board, design files, and how to import, download, and run an SDK example.   alex_yang_0-1758856779786.png   Hardware Requirements One FRDM-MCXE31B board A personal computer One USB Type-C cable   Software Requirements SDK25.06.00_FRDM-MCXE31B (Download from: https://mcuxpresso.nxp.com) MCUXpresso IDE v25.6 or later (Download from: MCUXpresso IDE | NXP) Serial Terminal Software for PC: Windows: PUTTY or Tera Term USB Device Driver Board User Manual The FRDM-MCXE31B board is a design and evaluation platform based on the NXP MCX E31B microcontroller (MCU). The MCX E31B MCU is based on an Arm Cortex-M7 core, running at speeds of up to 160 MHz with a 2.95 V–5.5 V supply. The FRDM-MCXE31B board includes: One MCX E31B device 64 Mbit external serial flash (Winbond) FXLS8974CFR3 I2C accelerometer sensor NMH1000 I2C magnetic switch Three TJA1057BTK CAN PHYs Ethernet PHY RGB LED Push buttons MCU-Link debug probe circuit The board is compatible with Arduino shield modules, Pmod boards, and mikroBUS. For debugging, the board uses an onboard (OB) debug probe, MCU-Link OB, based on the NXP LPC55S16 MCU. In this document, the MCX E31B is referred to as the target MCU, and the LPC55S16 as the debug MCU. This document provides detailed information about the FRDM-MCXE31B board interfaces, accelerometer, power supplies, clocks, connectors, jumpers, push buttons, LEDs, and the MCU-Link OB debug probe. You can download the FRDM-MCXE31B Board User Manual [UM12330] from: nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/frdm-development-board-for-mcx-e31-mcus:FRDM-MCXE31B   Getting Started The Getting Started page provides not only an introduction to the board but also instructions on how to import SDK projects. https://www.nxp.com/document/guide/getting-started-with-the-frdm-mcxe31b-board:GS-FRDM-MCXE31B   Documentation All documentation, datasheets and application notes can be found on the MCXE31 landing page: https://www.nxp.com/products/MCX-E31   Application Code Hub We provide several MCXE31B application code hub examples. You can find the project code from the following links and import them into MCUXpresso IDE to run:   https://github.com/nxp-appcodehub/an-digital-encoder-tamagawa-on-mcx31/tree/main Other ACH examples will be published soon.   Hands-on The following video demonstrates how to import, download, and run an SDK project using MCUXpresso IDE, using the Hello World example as a case study. please see attached video.  
記事全体を表示