DSC56800EX_Quick_Start_r2.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSC56800EX_Quick_Start_r2.6

ソリューションへジャンプ
2,590件の閲覧回数
antonio66
Contributor III

Hi,

On DSC56800EX_Quick_Start_r2.6 start up from the windows menu:

18983_18983.pngpastedImage_1.png

 

But I have this Error.

How to solve it ?

 

18982_18982.pngpastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 解決策
2,183件の閲覧回数
JardaP
NXP Employee
NXP Employee

Hello Antonio,

I can reproduce the issue.

The gct56F800.zip file contains update of the QuickStart GCT, which fixes the issue

Thegct_cfg_pinout.zip file contains update of peripherals and the pinout page for all derivates.

To apply the update unpack the files to <DSC56800EX_Quick_Start_r2.6_path>\tools\gct\

Best Regards,

Jaroslav

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,184件の閲覧回数
JardaP
NXP Employee
NXP Employee

Hello Antonio,

I can reproduce the issue.

The gct56F800.zip file contains update of the QuickStart GCT, which fixes the issue

Thegct_cfg_pinout.zip file contains update of peripherals and the pinout page for all derivates.

To apply the update unpack the files to <DSC56800EX_Quick_Start_r2.6_path>\tools\gct\

Best Regards,

Jaroslav

0 件の賞賛
返信