DSC56800EX_Quick_Start_r2.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSC56800EX_Quick_Start_r2.6

Jump to solution
2,613 Views
antonio66
Contributor III

Hi,

On DSC56800EX_Quick_Start_r2.6 start up from the windows menu:

18983_18983.pngpastedImage_1.png

 

But I have this Error.

How to solve it ?

 

18982_18982.pngpastedImage_0.png

Labels (1)
0 Kudos
Reply
1 Solution
2,206 Views
JardaP
NXP Employee
NXP Employee

Hello Antonio,

I can reproduce the issue.

The gct56F800.zip file contains update of the QuickStart GCT, which fixes the issue

Thegct_cfg_pinout.zip file contains update of peripherals and the pinout page for all derivates.

To apply the update unpack the files to <DSC56800EX_Quick_Start_r2.6_path>\tools\gct\

Best Regards,

Jaroslav

View solution in original post

0 Kudos
Reply
1 Reply
2,207 Views
JardaP
NXP Employee
NXP Employee

Hello Antonio,

I can reproduce the issue.

The gct56F800.zip file contains update of the QuickStart GCT, which fixes the issue

Thegct_cfg_pinout.zip file contains update of peripherals and the pinout page for all derivates.

To apply the update unpack the files to <DSC56800EX_Quick_Start_r2.6_path>\tools\gct\

Best Regards,

Jaroslav

0 Kudos
Reply