Flashing a MCF5272  with CFFlasher  CLI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing a MCF5272  with CFFlasher  CLI

ソリューションへジャンプ
2,273件の閲覧回数
meka_tama
Contributor I

Hi,

 

I am flashing a Coldfire MCF5272 with the CFFlasher 3.1.10 on Windows 7.

If i use the GUI everythings works fine, but when i try to get the same result with the CLI it doesn´t work.

I tried it with:

 

    CFFlasher.exe -t TARGET -p FILE -s -bdm PE_USB_ML

 

The programm tried to flash and it seems to work (no errors, just reports that the programm started and finished), but when I verify the result with the CFFlasher the data is just 0xFFFFFFFF.

It seems that only the erase works but not the programming.

There is an old discussion (https://community.freescale.com/thread/21082) with the same problem but there is no answer.

 

What may be the cause? If this is a problem in the CFFlasher, is there another programm to flash a MCF5272 (except the PROGCFZ)?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,002件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Well, the Cfflasher is quite old FSL free Flash Programming tool for FSL evaluation board. There really has problems & bugs with the CLI and for the reason that this tool is EOL now, so we have no resource to update the bug any more. (Anyway, the GUI is the recommend and should work without problem.)

Best Regards,

Fang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,003件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Well, the Cfflasher is quite old FSL free Flash Programming tool for FSL evaluation board. There really has problems & bugs with the CLI and for the reason that this tool is EOL now, so we have no resource to update the bug any more. (Anyway, the GUI is the recommend and should work without problem.)

Best Regards,

Fang

0 件の賞賛
返信
2,002件の閲覧回数
meka_tama
Contributor I

Thanks for the answer.

I tried to use the CFFlasher in a script, thats the reason i wanted the CLI. Now im abusing the GUI by simulating keyboard inputs with the win32api. Works quite well.

0 件の賞賛
返信