MCF52233 - polarity of the phy output led - LNKLED

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52233 - polarity of the phy output led - LNKLED

1,286件の閲覧回数
gilfine
Contributor II

Hi, I use MCF52233.

I an interested to invert the polarity of PHY led output (LNKLED) so that led is ON when link is not established and OFF otherwise.

Is there a way to do it ?

Thanks a lot,

Gil

ラベル(1)
2 返答(返信)

1,072件の閲覧回数
TomE
Specialist II

In a word, no. Not in software, unless you reprogram the pins as GPIO and drive them from code. In the case of the Link Led this would be trivially simple as it doesn't have to blink with traffic like the other ones do.

Otherwise just wire the LED to the other rail or add an inverter or transistor!

Tom

1,072件の閲覧回数
gilfine
Contributor II

Thanks a lot !

It was very helpful.

Gil

0 件の賞賛
返信