Differences between MC68020RC16E and MC68020CRC16E, except Ambient Operating Temperature ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences between MC68020RC16E and MC68020CRC16E, except Ambient Operating Temperature ?

Jump to solution
5,315 Views
patrickdivers
Contributor I

I don't find any documents about these differences;

Does anybody know or have information about this ?

 

Thancks,

Patrick

Labels (1)
0 Kudos
Reply
1 Solution
5,075 Views
miduo
NXP Employee
NXP Employee

Hello, Patrick

Please let me explain the "C" char here:

Blank -- 0°C to 70°C
C --  -40°C to 85°C
B --  -40°C to 70°C


There has no other difference between the two parts besides the operating temperature.


Best Regards,

Fang


View solution in original post

0 Kudos
Reply
3 Replies
5,076 Views
miduo
NXP Employee
NXP Employee

Hello, Patrick

Please let me explain the "C" char here:

Blank -- 0°C to 70°C
C --  -40°C to 85°C
B --  -40°C to 70°C


There has no other difference between the two parts besides the operating temperature.


Best Regards,

Fang


0 Kudos
Reply
5,072 Views
patrickdivers
Contributor I

Hello Fang,

Thanck for your response;

Is there a note that describe this ? and can you send me?

And what is the signification of the "E" char ? (CRC16E, RC16E)

Is there a note that describe this ? and can you send me?

Best Regards,

Patrick

0 Kudos
Reply
5,070 Views
miduo
NXP Employee
NXP Employee

Hi, Patrick

I am attaching you an old document, which you can find the information on page 9.