Flashing a MCF5272  with CFFlasher  CLI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flashing a MCF5272  with CFFlasher  CLI

跳至解决方案
1,542 次查看
meka_tama
Contributor I

Hi,

 

I am flashing a Coldfire MCF5272 with the CFFlasher 3.1.10 on Windows 7.

If i use the GUI everythings works fine, but when i try to get the same result with the CLI it doesn´t work.

I tried it with:

 

    CFFlasher.exe -t TARGET -p FILE -s -bdm PE_USB_ML

 

The programm tried to flash and it seems to work (no errors, just reports that the programm started and finished), but when I verify the result with the CFFlasher the data is just 0xFFFFFFFF.

It seems that only the erase works but not the programming.

There is an old discussion (https://community.freescale.com/thread/21082) with the same problem but there is no answer.

 

What may be the cause? If this is a problem in the CFFlasher, is there another programm to flash a MCF5272 (except the PROGCFZ)?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,271 次查看
miduo
NXP Employee
NXP Employee

Hi,

Well, the Cfflasher is quite old FSL free Flash Programming tool for FSL evaluation board. There really has problems & bugs with the CLI and for the reason that this tool is EOL now, so we have no resource to update the bug any more. (Anyway, the GUI is the recommend and should work without problem.)

Best Regards,

Fang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,272 次查看
miduo
NXP Employee
NXP Employee

Hi,

Well, the Cfflasher is quite old FSL free Flash Programming tool for FSL evaluation board. There really has problems & bugs with the CLI and for the reason that this tool is EOL now, so we have no resource to update the bug any more. (Anyway, the GUI is the recommend and should work without problem.)

Best Regards,

Fang

0 项奖励
回复
1,271 次查看
meka_tama
Contributor I

Thanks for the answer.

I tried to use the CFFlasher in a script, thats the reason i wanted the CLI. Now im abusing the GUI by simulating keyboard inputs with the win32api. Works quite well.

0 项奖励
回复