how to disable -t auto-detect when flashing using Codewarrior power architecture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to disable -t auto-detect when flashing using Codewarrior power architecture

1,214件の閲覧回数
dhkim
Contributor I

I'm using Codewarrior studio for Power Architecture

I'm just wanting to write elf program on Nor Flash device s29gl01gt11tfiv10

without address re-translation of elf format

just wanting to write an elf file image on flash memory 

I tried options that Flash programmer task offers

But

-t "Auto Detect"

doesn't disappear in console log

isn't there any way to disable "Auto detect" option when writing elf file?

0 件の賞賛
返信
1 返信

1,163件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

When you add “Program/Verify" Action, please specify the File Type as "Elf".

yipingwang_0-1672818538442.png

 

0 件の賞賛
返信