how to disable -t auto-detect when flashing using Codewarrior power architecture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to disable -t auto-detect when flashing using Codewarrior power architecture

1,756 Views
dhkim
Contributor I

I'm using Codewarrior studio for Power Architecture

I'm just wanting to write elf program on Nor Flash device s29gl01gt11tfiv10

without address re-translation of elf format

just wanting to write an elf file image on flash memory 

I tried options that Flash programmer task offers

But

-t "Auto Detect"

doesn't disappear in console log

isn't there any way to disable "Auto detect" option when writing elf file?

0 Kudos
Reply
1 Reply

1,705 Views
yipingwang
NXP TechSupport
NXP TechSupport

When you add “Program/Verify" Action, please specify the File Type as "Elf".

yipingwang_0-1672818538442.png

 

0 Kudos
Reply