CW_ARMv8 TAP connection with Linux host: no probes found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW_ARMv8 TAP connection with Linux host: no probes found

1,625 Views
Ray_33
Contributor II

Target connection device: LS1088A_RDB; Linux OS: ubuntu 20.04.4; CodeWarrior: CW4NET_v2020.06. Tried to connect the target board to debug a demo project thru the CWTAP, and followed the below instruction:

https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Issue-in-code-warrior-for-connecting-to-target-us...

%config cc cwtap:

maximum number of Command Converters reached

config fail

%show cc

0: USB open failure

there are no command converters configured

CWTAP LED status: TX/RX is flashing green, RUN/PAUSE orange.

Let me know any advice or any further information needed. Thanks.

 

0 Kudos
Reply
1 Reply

1,574 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached resolution.

0 Kudos
Reply