e500 SDK install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,904件の閲覧回数
ashwingandhi
Contributor II

we need to load Linux to p1013 processor a customized board.

I have downloaded the SDK for e500 core, CodeWrrior for PowerPC and also we have USB TAP.

But am unable to understand how to install SDK and build images that can be loaded to the target board.

Please let me know any tutorial or at least steps available for that.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,313件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ashwin Gandhi,

Please download and install QorIQ Linux SDK 1.9 Source and Cache ISO for e500v2 processors from Linux® SDK for QorIQ Processors|NXP​. Please refer to the document QorIQ Linux SDK 1.6 Working With Yocto .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,314件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ashwin Gandhi,

Please download and install QorIQ Linux SDK 1.9 Source and Cache ISO for e500v2 processors from Linux® SDK for QorIQ Processors|NXP​. Please refer to the document QorIQ Linux SDK 1.6 Working With Yocto .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,313件の閲覧回数
mindchasers
Contributor III

And definitely check out the Yocto Quick Start manual (yocto-project-qs.html)  located inside the SDK source ISO at

sdk_documentation/pdf/yocto/yocto_quick_start

0 件の賞賛
返信
2,313件の閲覧回数
mindchasers
Contributor III

Hi Ashwin,

Look at the contents of the QorIQ SDK V1.9 source ISO, and you will see in the root the SDK manual: QorIQ-SDK-1.9-IC-RevA.pdf.  There is also a directory titled sdk_documentation that contains many other documents including the yocto project docs. 

Keep in mind that the SDK utilizes the Yocto Project as its foundation for building the Linux distribution.  Therefore, you may want to join the project's mailing lists and look at its Wiki in addition to the official docs: yoctoproject.org

Good luck,

Bob

0 件の賞賛
返信