QorIQ Linux SDK 1.6 Working With Yocto

Document created by Yiping Wang Employee on Oct 7, 2014
Version 1Show Document
  • View in full screen mode

This application note introduces how to install and use Yocto to customize and generate required images.

QorIQ SDK 1.6 installation and build environment setting up procedures.

Using script fsl-setup-poky to create a build project and explaining specific parameters related with local configuration file.


Yocto Image types and generation, and how to modify variables in machine configuration file to generate required images.


How to run specific bitbake tasks, and how to configure and rebuild u-boot and Linux Kernel.


How to create customized rootfs image recipes to add and remove packages list, use ROOTFS_POSTPROCESS_COMMAND to modify RFS content before image generation.


Using merge-files package to add users’ own files into root file system.


Creating new package recipes in Yocto build environment.

1 person found this helpful