QCVS install error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
12,514件の閲覧回数
mohsenhaghighat
Contributor III

when I install QCVS in eclipse. this error has been occurred.

I use QCVS for qoriq power version 4.5.0.00001 . the eclipse version is "Eclipse IDE for C/C++ Developers 4.4.2".

Any body can help me.

 

An error occurred while collecting items to be installed

session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.freescale.qcvs.feature_root 4.5.0.0001-20160210, action=).

The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
10,175件の閲覧回数
addiyi
NXP Employee
NXP Employee

The correct update site for installing QCVS + FSL Updater is http://freescale.com/lgfiles/updates/Eclipse/QCVS for only ARM support or http://freescale.com/lgfiles/updates/Eclipse/QCVS_PA​ for QCVS 4.5 release including ARM + PA support.

Please refer to QCVS Installation Guide, chapter 3.2.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
10,175件の閲覧回数
florentinbourge
Contributor II

I had a similar problem with the same error message ! Juno 4.2 + QCVS for qoriq power version 4.5.0.00001

So I follow advices fromaddiyi‌ which are good, but I omited to install the "Eclipse Freescale Solutions Category" first. That was my second problem.

So,

  1. Add a new repository into eclipse : Help -> Install New Software :
  2. Firstly install : Eclipse Freescale Solutions Category, only ! -> Restart eclipse.
  3. Secondly install the : QorIQ Configuration and Validation Suite 4.5. -> Restart eclipse

Everything work fine .

0 件の賞賛
返信
10,175件の閲覧回数
addiyi
NXP Employee
NXP Employee

Did you install first "Eclipse Freescale Solutions Category"?

Adrian

10,175件の閲覧回数
mohsenhaghighat
Contributor III

Hi

I use eclipse 4.2 Juno.

I find "Eclipse Freescale Solutions Category" at Processor Expert Software, Microcontroller Driver S|NXP  and install it.

and then I try to install QCVS but it error "No action found for: com.freescale.updater.customActions.freescaleprocesscheck."

I cant use from this link : http://freescale.com/lgfiles/updates/Eclipse/QCVS_PA .

I think that  "Eclipse Freescale Solutions Category" has mistake. where can I download it?

0 件の賞賛
返信
10,176件の閲覧回数
addiyi
NXP Employee
NXP Employee

The correct update site for installing QCVS + FSL Updater is http://freescale.com/lgfiles/updates/Eclipse/QCVS for only ARM support or http://freescale.com/lgfiles/updates/Eclipse/QCVS_PA​ for QCVS 4.5 release including ARM + PA support.

Please refer to QCVS Installation Guide, chapter 3.2.

Adrian

0 件の賞賛
返信
9,452件の閲覧回数
Kernelhacker
Contributor III

How do we access this locations?

getting "Page not found"

0 件の賞賛
返信
9,403件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

This can only be access using the CodeWarrio SW under Help > Install new SW

0 件の賞賛
返信
9,401件の閲覧回数
Kernelhacker
Contributor III

OK, thanks.

But I was trying to integrate with eclipse. Isn't that possible by any means?

0 件の賞賛
返信
9,396件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport
  1. Inside of the CodeWarrior Tools click on Help > Install New Software
  2. You will see the updates that are abaiable for your software
  3. Can you send a Screen capture of what you see please.
0 件の賞賛
返信