Configuration file for LS1012ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuration file for LS1012ARDB

跳至解决方案
1,982 次查看
nattapongsungch
Contributor III

Hi i'm working on LS1012ARDB with codeWarrior for recovery and program QSPI.

 

I downloaded CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.2 and already updated by inside (Help -> check for update).

 

So ,I cannot find LS1012ARDB on Target connection.

 

165259_165259.pngScreenshot from 2016-09-30 11_37_29.png

 

Thank you

Nattapong

标签 (1)
0 项奖励
回复
1 解答
1,691 次查看
addiyi
NXP Employee
NXP Employee

Check for Updates is not working property. It will not update plug-ins that add support for LS1012. Please use Help > Install New Software instead, and select ARMv8 Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/11.2.0/com.freescale.armv8_win as update site in Work with field.

Adrian

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,692 次查看
addiyi
NXP Employee
NXP Employee

Check for Updates is not working property. It will not update plug-ins that add support for LS1012. Please use Help > Install New Software instead, and select ARMv8 Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/11.2.0/com.freescale.armv8_win as update site in Work with field.

Adrian

0 项奖励
回复
1,691 次查看
justinjonas
Contributor III

The update site for this is down. Do you know if it will be back up soon?

0 项奖励
回复
1,691 次查看
nattapongsungch
Contributor III

Thank you , It's work.

0 项奖励
回复