Configuration file for LS1012ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuration file for LS1012ARDB

ソリューションへジャンプ
1,988件の閲覧回数
nattapongsungch
Contributor III

Hi i'm working on LS1012ARDB with codeWarrior for recovery and program QSPI.

 

I downloaded CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.2 and already updated by inside (Help -> check for update).

 

So ,I cannot find LS1012ARDB on Target connection.

 

165259_165259.pngScreenshot from 2016-09-30 11_37_29.png

 

Thank you

Nattapong

ラベル(1)
0 件の賞賛
返信
1 解決策
1,697件の閲覧回数
addiyi
NXP Employee
NXP Employee

Check for Updates is not working property. It will not update plug-ins that add support for LS1012. Please use Help > Install New Software instead, and select ARMv8 Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/11.2.0/com.freescale.armv8_win as update site in Work with field.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,698件の閲覧回数
addiyi
NXP Employee
NXP Employee

Check for Updates is not working property. It will not update plug-ins that add support for LS1012. Please use Help > Install New Software instead, and select ARMv8 Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/11.2.0/com.freescale.armv8_win as update site in Work with field.

Adrian

0 件の賞賛
返信
1,697件の閲覧回数
justinjonas
Contributor III

The update site for this is down. Do you know if it will be back up soon?

0 件の賞賛
返信
1,697件の閲覧回数
nattapongsungch
Contributor III

Thank you , It's work.

0 件の賞賛
返信