streamb.h default has syntax issues?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

streamb.h default has syntax issues?

跳至解决方案
2,391 次查看
isaacgainey
Contributor I

Hello, I am runing MCU v10.6 offline eclipse edition. I have started a C++ -> RS08 project however when I go to build / run it, one of the files "streamb.h" appears with around 40 syntax errors. I have not touched this file, so my question would have to be is there an update that fixes this or is there a setting that is either enable or disable that shouldn't be? Or prehaps is there a fix existing that is simply buried?

 

edit : Also, the most common syntax issue is CS801 ";" missing even though there exist where they should.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,286 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

can you please upload your project so that we can check the problem directly on my side?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,287 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

can you please upload your project so that we can check the problem directly on my side?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,286 次查看
isaacgainey
Contributor I

https://drive.google.com/file/d/0B-A3z2bCi6RYMjA4TXdlNkRlQ1U/view?usp=sharing

Here are the files you requested.

Thank you,

Isaac Gainey

0 项奖励
回复