streamb.h default has syntax issues?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

streamb.h default has syntax issues?

Jump to solution
2,458 Views
isaacgainey
Contributor I

Hello, I am runing MCU v10.6 offline eclipse edition. I have started a C++ -> RS08 project however when I go to build / run it, one of the files "streamb.h" appears with around 40 syntax errors. I have not touched this file, so my question would have to be is there an update that fixes this or is there a setting that is either enable or disable that shouldn't be? Or prehaps is there a fix existing that is simply buried?

 

edit : Also, the most common syntax issue is CS801 ";" missing even though there exist where they should.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,353 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

can you please upload your project so that we can check the problem directly on my side?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,354 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

can you please upload your project so that we can check the problem directly on my side?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,353 Views
isaacgainey
Contributor I

https://drive.google.com/file/d/0B-A3z2bCi6RYMjA4TXdlNkRlQ1U/view?usp=sharing

Here are the files you requested.

Thank you,

Isaac Gainey

0 Kudos
Reply