streamb.h default has syntax issues?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

streamb.h default has syntax issues?

ソリューションへジャンプ
2,454件の閲覧回数
isaacgainey
Contributor I

Hello, I am runing MCU v10.6 offline eclipse edition. I have started a C++ -> RS08 project however when I go to build / run it, one of the files "streamb.h" appears with around 40 syntax errors. I have not touched this file, so my question would have to be is there an update that fixes this or is there a setting that is either enable or disable that shouldn't be? Or prehaps is there a fix existing that is simply buried?

 

edit : Also, the most common syntax issue is CS801 ";" missing even though there exist where they should.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,349件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

can you please upload your project so that we can check the problem directly on my side?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,350件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

can you please upload your project so that we can check the problem directly on my side?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,349件の閲覧回数
isaacgainey
Contributor I

https://drive.google.com/file/d/0B-A3z2bCi6RYMjA4TXdlNkRlQ1U/view?usp=sharing

Here are the files you requested.

Thank you,

Isaac Gainey

0 件の賞賛
返信