Where can I get the technical notes?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where can I get the technical notes?

跳至解决方案
2,756 次查看
wangyanjun
Contributor II
Where can I download the technical notes? I'm using the Codewarrior for hcs12, and the manual list some technical notes number such as TN238, TN240. But I can't find them. Where can I get them. Thanks!
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,588 次查看
mayfly
Contributor III
I had quite a time trying to find the technical notes until I came upon this thread.  Tried googling and a search on freescale for the specific Technical note (tn100)...but nothing came up.   A bit frustrating...I think someone should fix that somewhere. 

Here's the direct link:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_816-bit_Technical_Notes_SP.exe?fps...

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,589 次查看
mayfly
Contributor III
I had quite a time trying to find the technical notes until I came upon this thread.  Tried googling and a search on freescale for the specific Technical note (tn100)...but nothing came up.   A bit frustrating...I think someone should fix that somewhere. 

Here's the direct link:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_816-bit_Technical_Notes_SP.exe?fps...
0 项奖励
回复
1,588 次查看
Lundin
Senior Contributor IV
When you installed CW there should have been an option to include them. Otherwise they can be found in pdf format on the CW cd.
0 项奖励
回复
1,588 次查看
CrasyCat
Specialist III
Hello
 
You can download the Technical Notes from the Web as follows:
 
  - Click on the link "HC(S)08/RS08 Microcontrollers"
  - Click on the tab "Documentation"
  - Click on the link "816TNSP"
 
You should then get the .zip file containing the technical notes.
 
CrasyCat
 
0 项奖励
回复