Where can I get the technical notes?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I get the technical notes?

Jump to solution
2,767 Views
wangyanjun
Contributor II
Where can I download the technical notes? I'm using the Codewarrior for hcs12, and the manual list some technical notes number such as TN238, TN240. But I can't find them. Where can I get them. Thanks!
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,599 Views
mayfly
Contributor III
I had quite a time trying to find the technical notes until I came upon this thread.  Tried googling and a search on freescale for the specific Technical note (tn100)...but nothing came up.   A bit frustrating...I think someone should fix that somewhere. 

Here's the direct link:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_816-bit_Technical_Notes_SP.exe?fps...

View solution in original post

0 Kudos
Reply
3 Replies
1,600 Views
mayfly
Contributor III
I had quite a time trying to find the technical notes until I came upon this thread.  Tried googling and a search on freescale for the specific Technical note (tn100)...but nothing came up.   A bit frustrating...I think someone should fix that somewhere. 

Here's the direct link:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_816-bit_Technical_Notes_SP.exe?fps...
0 Kudos
Reply
1,599 Views
Lundin
Senior Contributor IV
When you installed CW there should have been an option to include them. Otherwise they can be found in pdf format on the CW cd.
0 Kudos
Reply
1,599 Views
CrasyCat
Specialist III
Hello
 
You can download the Technical Notes from the Web as follows:
 
  - Click on the link "HC(S)08/RS08 Microcontrollers"
  - Click on the tab "Documentation"
  - Click on the link "816TNSP"
 
You should then get the .zip file containing the technical notes.
 
CrasyCat
 
0 Kudos
Reply