This reference manual describes the contents of the Embedded Warrior Library for C++. The C++ Standard library provides an extensible framework, and contains components for: language support, diagnostics, general utilities, strings, locales, containers, iterators, algorithms, numerics, and input/output. Additionally, EWL C++ offers extra facilities forinput/output, threads, and other components. Libraries included within this reference manual are: The EWL C++ Library Overview of thismanual describes the language support library that provides components that are required by certain parts of the C++ language, such as memory allocation and exception processing. “LanguageSupport Library” discusses the ANSI/ISO language support library. Diagnostics Library elaborates on the diagnostics library that provides a consistent framework for reporting errorsina C++ program, including predefined exception classes. General Utilities Libraries discusses the general utilities library, which includes components used by other library elements, such as predefined storage allocator for dynamic storage management. Strings Library discusses the strings components provided for manipulating text represented as sequences of type char, sequences of typewchar_t, or sequences of any other “character-like” type. Localization Library covers the localization components extend internationalization support for character classification, numeric, monetary, anddate/time formatting and parsing among other things. EWL_Utility utilities used for non standard headers. Overview of EWL C++ Debug Mode describes the Embedded Warrior Library for C++ debug mode facilities. Hash Libraries describes nonstandard “hash” libraries. Metrowerks::threads is a reference to threads support in the Embedded WARRIOR Libraries. EWL std::tr1 is a reference about items that are proposed for inclusion in the Embedded Warrior Library C++ Switches, Flags and Defines is a chapter on the various flags that you can use to create a customized version of the EWL C++ Library ...and many more resourceful subjects are contained! Get ready to update your CodeWarrior Development Tools for EWL C++ programming! View manual here!
View full article