Help porting classic project to CodeWarrior 11.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help porting classic project to CodeWarrior 11.1

2,640件の閲覧回数
lpeterso
Contributor I

What is the best way to migrate a ColdFire v1 project made in classic CodeWarrior to CodeWarrior 11.1?

0 件の賞賛
返信
3 返答(返信)

2,494件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

 

Please take a look to my colleagues response in the below thread, he expalins the steps needed to migrate from CW for Coldfire V6.2 to CodeWarrior 10.6 but the same applies for CodeWarrior 11:

 

https://community.nxp.com/thread/379597#comment-585434 


Hope it helps!

 

Best Regards,

Soledad

0 件の賞賛
返信

2,494件の閲覧回数
lpeterso
Contributor I

I have been following this guide http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf and have run into some problems. I created a new project, moved the files from the classic project to the new one, and updated the paths, however, when I build I get a "link failed" error. Any help would be appreciated.

specifically the errors I am getting are

"Link Failed",

"mingw32-make. ***[thermal_coldfire_port.elf] Error 1",

"Undefined : "_BDT_BASE" Referenced from "_usb_send" ", and

"Undefined : "_IPSBAR" Referenced from "_usb_receive"


0 件の賞賛
返信

2,494件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

You need to do some ports from the CW classic to CW 11, there is no direct process.

Please check the following thread:

https://community.nxp.com/thread/379597 

Have a nice day!

Regards

Soledad

0 件の賞賛
返信