FRWY LS1012A Test OCRAM memory access failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRWY LS1012A Test OCRAM memory access failed

5,828件の閲覧回数
henryk_paluch
Contributor I

Hello!

I'm trying to connect CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA Version: 11.4.1 Build Id: 190423 to board FRWY LS1012A with 512MB DDR using CMSIS-DAP connection. When I click on "Diagnose Connection" nearly all tests pass, but "Test OCRAM memory access" fails with:

Cannot write data at address 0x10000000

The board is fully functional (there is U-Boot "firmware_ls1012afrwy_512mb_uboot_qspiboot.img"

from LSDK19.03 in QSPI NOR, and "Linux NXP-LSDK 19.03" on microSD card). 

test-ocram-failed.png

The CodeWarrior was installed from "CW_ARMv8_v2019.01_b190130_Win_Offline.exe" and updated on Jun 4 2019 using Help -> Check for Updates.

タグ(3)
0 件の賞賛
返信
8 返答(返信)

5,554件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Henryk Paluch,

I created a bareboard project in CodeWarrior for ARMv8(Version: 11.4.1 Build Id: 190423), duplicated and edited target connection for LS1012A_FRWY, then connect to LS1012AFRWY board and read OCRAM memory address 0x10000000 without any problem.

Please refer to sections "3.2.1 Creating, building bareboard project" and "3.2.2 Debugging bareboard project" in CW4NET_v2019.01\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf to create and debug the bareboard project.

Did you modify CodeWarrior initialization file?  If yes, please also send your modified CW initialization file to me to do more investigation?

Please check whether this problem remains when using the hard-coded RCW? Please modify "USE_SAFE_RCW = True" in CodeWarrior initialization to do verification.

In addition, would you please capture the CCS protocol console log to me to do more investigation?

Before connect to the target board, in CodeWarrior IDE please open "PROTOCOL logging" panel from Window->Preferences->Debug Server Configuration->Logging Configuration, please specify "Logging Level" as "DEBUG"and check "Enable logging to Eclipse console", please open the console panel from Window->Show View->Console.

Please connect to the target board, the detailed CCS low level communication log will be printed in Protocol logging Console, please capture this log to me to do more investigation.

If the CCS log doesn't display, please click "Display Select Console" icon at the right top of the Console panel to select Protocol logging Console.

Thanks,

Yiping

0 件の賞賛
返信

5,554件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Henryk Paluch,

There is problem at writing register to set rcw_src to hard-coded RCW option in your CCS log.

According to your original description, there is valid RCW on your target board, please configure "USE_SAFE_RCW = False" in the default CW initialization file(without any modification) to check whether the CodeWarrior bare board project can connect to the target board with valid RCW on NOR flash.

If the connection problem remains, please capture the CCS log to me again.

Thanks,

Yiping

0 件の賞賛
返信

5,554件の閲覧回数
henryk_paluch
Contributor I

Hello!

In such case (USE_SAFE_RCW = False) I receive OCRAM access error (as described in my initial post).

The error entries in Console are:

ccs_get_cc_config
 serverh = 0
 cc = 0
 config_string =
 ccs_get_cc_config; ccs_error = 23
 Error message: CC not present

...

ccs_write_memory
 coreh = [serverh:0;cc_index:0;chain_pos:10]
 addr = [space:0;size:1;address_hi:0x00000000;address_lo:0x10000000]
 data: (size = 8)
   12345678 9ABCDEF0
 ccs_write_memory; ccs_error = 5
 Error message: Core not responding

Complete Console log and screenshot is attached below in file error1.zip

(Reminder - I use "CMSIS-DAP" connection, not TAP).

Best regards

 --hp

0 件の賞賛
返信

5,554件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Henryk Paluch,

Did you modify CodeWarrior initialization file? Please use the default one in the bareboard project to connect to the target board.

 

Please refer to my attached CCS log connecting FRWY LS1012A, it doesn't contain the section to write OCRAM memory, I didn't find the section to write OCRAM memory 0x10000000 in my CCS log. The program will be downloaded to DDR memory at 0x80000000.

ccs_write_memory
 coreh = [serverh:0;cc_index:0;chain_pos:10]
 addr = [space:0;size:1;address_hi:0x00000000;address_lo:0x10000000]


If your problem remains, you could send your CodeWarrior project to me, I will verify it to connect to my target board.

Thanks,

Yiping

0 件の賞賛
返信

5,554件の閲覧回数
henryk_paluch
Contributor I

Hello!

I rather reinstalled whole CodeWarrior + latest updates (using Help -> Check for Updates in CW) to ensure clean environment. The OCRAM error is same as described in initial post.

To reproduce this error, just "Target Connections" View is needed (it is not project specific - therefore I did not create/attached project files). Here is description of attached zip archive files:

File frwy-connection-files.zip:

- frwy-connection-files\Config-boards\LS1012A_FRWY.tcc and LS1012A_FRWY_init.py - original system files from c:\Freescale\CW4NET_v2019.01\CW_ARMv8\Config\boards\

- frwy-connection-files\CW-exports\LS1012A_FRWY.tcc - export of original LS1012 FRWY connection (TAP) from "Target Connections" View

- frwy-connection-files\CW-exports\LS1012A_FRWY_custom2.tcc - export of my customized connection from "Target Connections" View - the only difference is the use of CMSIS-DAP instead of TAP (thus only probe index changed)

NOTE: The "Export" function updates timestamp on exported files :smileyalert:. It is the reason why (unmodified) file frwy-connection-files\Config-boards\LS1012A_FRWY.tcc has recent timestamp (July 8).

File: CodeWarrior-configuration.zip:

CodeWarrior-configuration.txt complete CodeWarrior configuration including installed components from Help -> About -> Installation Details -> Configuration tab.

Best regards

  --Henryk Paluch

0 件の賞賛
返信

5,554件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that you are using the OCRAM version project, please try the attached workspace, please open CodeWarrior IDE and specify the workspace path as the attached folder.

0 件の賞賛
返信

5,554件の閲覧回数
henryk_paluch
Contributor I

Hello!

Unfortunately I get same OCRAM error with provided workspace. Also the 2 errors in Console view are same (see attached console.zip). According to official data sheets the LS1012A contains OCRAM and it seems to be used as buffer (for example for reading/writing NOR flash from/to PC). So it is probably not meaningful to attempt to just ignore OCRAM.

Anyway - feel free to close this issue. My trial is expiring and I have currently other tasks in my queue.

Best regards

  --Henryk Paluch

ls1012afrwy-ws-ocram-error.png

0 件の賞賛
返信

5,327件の閲覧回数
henryk_paluch
Contributor I

Hello all!

There is one thing different on my FRWY board - it uses TF-A based firmware (because it is the only supported one from LSDK 18.12+). However original FRWY board used PPA firmware. I know from my experience that TF-A by default denies OCRAM access to any non EL3 code (including U-Boot and Linux kernel).

 

Could be that cause of OCRAM access errors - when on-board CMSIS-DAP is used with TF-A firmware in QSPI NOR flash?

 

Best regards

  --Henryk Paluch

0 件の賞賛
返信