Problem:Icu configuration about MCAL4_3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem:Icu configuration about MCAL4_3

ソリューションへジャンプ
7,090件の閲覧回数
Ada_Lovelace
Contributor IV

Dear all,

I have a problem, it has an error when I use the demo about  lightning_MPC5777C_4.3_Split.

The demo is based on AUTOSAR\MPC5777C_MCAL4_3_RTM_1_0_0\MPC5777C_MCAL4_3_RTM_1_0_0_Sample_Application.

The problem is about the ICU configuration, I can not choose the 'ICU_MODE_SIGNAL_MEASUREMENT',it tells me that I must enable the IcuSignalMeasurement optional container, but I can not find the way to enable it.

Could anybody can tell me, how to solve the problem?

thanks.

pastedImage_1.png

pastedImage_2.png

タグ(3)
0 件の賞賛
返信
1 解決策
7,003件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

Hope this helps,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
6,943件の閲覧回数
eleanor
Contributor I

Follow this steps

1. Edge detection uses ECNT instruction. Please refer to N2HET instruction set in TRM

2. Signal measurement (duty, Period): use PCNT instruction. Please refer to N2HET instruction set in TRM.

0 件の賞賛
返信
7,004件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

Hope this helps,

Marius

0 件の賞賛
返信