Problem:Icu configuration about MCAL4_3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem:Icu configuration about MCAL4_3

Jump to solution
6,291 Views
Ada_Lovelace
Contributor IV

Dear all,

I have a problem, it has an error when I use the demo about  lightning_MPC5777C_4.3_Split.

The demo is based on AUTOSAR\MPC5777C_MCAL4_3_RTM_1_0_0\MPC5777C_MCAL4_3_RTM_1_0_0_Sample_Application.

The problem is about the ICU configuration, I can not choose the 'ICU_MODE_SIGNAL_MEASUREMENT',it tells me that I must enable the IcuSignalMeasurement optional container, but I can not find the way to enable it.

Could anybody can tell me, how to solve the problem?

thanks.

pastedImage_1.png

pastedImage_2.png

Tags (3)
0 Kudos
Reply
1 Solution
6,204 Views
mariuslucianand
NXP Employee
NXP Employee

Hello cuihan.ma@dotrustech.com‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

Hope this helps,

Marius

View solution in original post

0 Kudos
Reply
2 Replies
6,144 Views
eleanor
Contributor I

Follow this steps

1. Edge detection uses ECNT instruction. Please refer to N2HET instruction set in TRM

2. Signal measurement (duty, Period): use PCNT instruction. Please refer to N2HET instruction set in TRM.

0 Kudos
Reply
6,205 Views
mariuslucianand
NXP Employee
NXP Employee

Hello cuihan.ma@dotrustech.com‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

Hope this helps,

Marius

0 Kudos
Reply