S08SG micro reset characteristics

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S08SG micro reset characteristics

765 次查看
pratikp1
Contributor I

I am working on the S08SG microcontroller. What is the effect on the state of the port pins if the Reset line is held low for a considerable duration of time (For e.g. if it is accidently short circuited to Ground). Also, does the micro keep resetting multiple times for the entire duration when the reset line is pulled to low(as it is a low level triggered reset) or it resets just once when the reset line goes high again?

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

685 次查看
Stano
NXP Employee
NXP Employee

The reset line force the MCU pins to the high impedance when pulled low. The MCU will reset only once, when the reset lines goes high.

0 项奖励
回复