S08SG micro reset characteristics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08SG micro reset characteristics

1,242 Views
pratikp1
Contributor I

I am working on the S08SG microcontroller. What is the effect on the state of the port pins if the Reset line is held low for a considerable duration of time (For e.g. if it is accidently short circuited to Ground). Also, does the micro keep resetting multiple times for the entire duration when the reset line is pulled to low(as it is a low level triggered reset) or it resets just once when the reset line goes high again?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,162 Views
Stano
NXP Employee
NXP Employee

The reset line force the MCU pins to the high impedance when pulled low. The MCU will reset only once, when the reset lines goes high.

0 Kudos
Reply