PWM on FTM2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PWM on FTM2

跳至解决方案
2,724 次查看
pramodtm-b46240
Contributor III

Hi,

     I'm using MC9S08PT60 controller to generate a PWM using FTM2, using processor expert.I could generate the same on FTM0 and FTM1 and also could vary the duty cycle. But i want it on FTM2 so that I can control the speed of a DC motor, owing to the advantage that FTM2 supports complementary channels.Can anybody help on this?

 

Thanks,

标签 (1)
0 项奖励
回复
1 解答
2,437 次查看
pramodtm-b46240
Contributor III

Thank u very much...

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,437 次查看
weapon
Senior Contributor I

Hi,

We have a bldc motor demo in TWR-S08PT, whihc uses FTM2 to generate 6 pwm signal to control a bldc motors. you can take it as reference.

The demo is in attachment.  Hope it can be helpful.

2,438 次查看
pramodtm-b46240
Contributor III

Thank u very much...

0 项奖励
回复