Thank you fore the sanded link, what these symbol describes, but these answers leads to mine fundamental question.
I'v the following code lines
staa InBetrieb
beq no_busy ;jumps if Z=1
jmp in_busy ;running!
where I've seen the second code line only branches if the staa-instruction Z sets to 1.
So do I read, to the instruction "staa", the lines
Z X7• X6 • X5 • X4 • X3 • X2 • X1 • X0
Set if result is $00; cleared otherwise.
in the RM, where for me the question appears what the "result" - of a staa-instruction - is?
I could imagine that the result $00 is, if for example the argument of the instruction a valid one is,
but I couldn't see these explanation on page 579 of the pdf-description.
So, when is the result of a staa-instruction $00?
I couldn't imagine that that result the value of accumulator a describes.