PWM on FTM2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM on FTM2

Jump to solution
2,852 Views
pramodtm-b46240
Contributor III

Hi,

     I'm using MC9S08PT60 controller to generate a PWM using FTM2, using processor expert.I could generate the same on FTM0 and FTM1 and also could vary the duty cycle. But i want it on FTM2 so that I can control the speed of a DC motor, owing to the advantage that FTM2 supports complementary channels.Can anybody help on this?

 

Thanks,

Labels (1)
0 Kudos
Reply
1 Solution
2,565 Views
pramodtm-b46240
Contributor III

Thank u very much...

View solution in original post

0 Kudos
Reply
2 Replies
2,565 Views
weapon
Senior Contributor I

Hi,

We have a bldc motor demo in TWR-S08PT, whihc uses FTM2 to generate 6 pwm signal to control a bldc motors. you can take it as reference.

The demo is in attachment.  Hope it can be helpful.

2,565 Views
pramodtm-b46240
Contributor III

Thank u very much...

0 Kudos
Reply