Undesired FLASH protection on MC9S08QB4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Undesired FLASH protection on MC9S08QB4

跳至解决方案
1,617 次查看
benthie
Contributor II

Hey everybody,

 

my current application uses the flash programming routines from AN3942. At some point my program writes data to the flash (0xFFC0 - 0xFFFF). Everything works fine so far, the data is where I want it to be and when I debug the controller, the FOPT register tells me, that the flash is unsecured (FOPT = 0xC2).

 

If I stop my program and debug it again, then the "device is secured"-dialog pops up.

 

Does anybody has an idea, at which point the securing happens?

 

Regards,

Ben

标签 (1)
0 项奖励
回复
1 解答
1,517 次查看
benthie
Contributor II

I found the problem. I erased the NVOPT bits due to a page erase and did not set the SEC00 bit back to 0. Ref.Manual p.55.

Thank you anyway.

Ben

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,518 次查看
benthie
Contributor II

I found the problem. I erased the NVOPT bits due to a page erase and did not set the SEC00 bit back to 0. Ref.Manual p.55.

Thank you anyway.

Ben

0 项奖励
回复