PWM on FTM2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,852件の閲覧回数
pramodtm-b46240
Contributor III

Hi,

     I'm using MC9S08PT60 controller to generate a PWM using FTM2, using processor expert.I could generate the same on FTM0 and FTM1 and also could vary the duty cycle. But i want it on FTM2 so that I can control the speed of a DC motor, owing to the advantage that FTM2 supports complementary channels.Can anybody help on this?

 

Thanks,

ラベル(1)
0 件の賞賛
返信
1 解決策
2,565件の閲覧回数
pramodtm-b46240
Contributor III

Thank u very much...

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,565件の閲覧回数
weapon
Senior Contributor I

Hi,

We have a bldc motor demo in TWR-S08PT, whihc uses FTM2 to generate 6 pwm signal to control a bldc motors. you can take it as reference.

The demo is in attachment.  Hope it can be helpful.

2,565件の閲覧回数
pramodtm-b46240
Contributor III

Thank u very much...

0 件の賞賛
返信