Debugger & flash programmer in CW 10.4 for HCS08: different result

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugger & flash programmer in CW 10.4 for HCS08: different result

跳至解决方案
2,619 次查看
damorin
Contributor I

Hi everyone,

everything is working fine when the target is programmed using the debugger but as soon as the flash programmer is used, the target is no more booting.

We disabled all checksum, remove the watchdog but no result.

We are using PE Mircom USB Multilink and also the newer one; same result.

We also tried with CW 6.2 and same result too with the flash programmer.

Any hint on what to look next ?

Thanks in advance,

Robert

 

 

0 项奖励
回复
1 解答
2,610 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Can you give me a little bit more details? 

 

this is with any project or only with a specific one?

 

regards

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,611 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Can you give me a little bit more details? 

 

this is with any project or only with a specific one?

 

regards

 

0 项奖励
回复
2,603 次查看
damorin
Contributor I

 

Hi, 

now it's working; it was two problems from two different sources (wrong CW version and a bug in the code).

Happy to say 'not a bug'.

 

0 项奖励
回复