Debugger & flash programmer in CW 10.4 for HCS08: different result

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger & flash programmer in CW 10.4 for HCS08: different result

Jump to solution
2,614 Views
damorin
Contributor I

Hi everyone,

everything is working fine when the target is programmed using the debugger but as soon as the flash programmer is used, the target is no more booting.

We disabled all checksum, remove the watchdog but no result.

We are using PE Mircom USB Multilink and also the newer one; same result.

We also tried with CW 6.2 and same result too with the flash programmer.

Any hint on what to look next ?

Thanks in advance,

Robert

 

 

0 Kudos
Reply
1 Solution
2,605 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Can you give me a little bit more details? 

 

this is with any project or only with a specific one?

 

regards

 

View solution in original post

0 Kudos
Reply
2 Replies
2,606 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Can you give me a little bit more details? 

 

this is with any project or only with a specific one?

 

regards

 

0 Kudos
Reply
2,598 Views
damorin
Contributor I

 

Hi, 

now it's working; it was two problems from two different sources (wrong CW version and a bug in the code).

Happy to say 'not a bug'.

 

0 Kudos
Reply