Debugger & flash programmer in CW 10.4 for HCS08: different result

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger & flash programmer in CW 10.4 for HCS08: different result

ソリューションへジャンプ
3,426件の閲覧回数
damorin
Contributor I

Hi everyone,

everything is working fine when the target is programmed using the debugger but as soon as the flash programmer is used, the target is no more booting.

We disabled all checksum, remove the watchdog but no result.

We are using PE Mircom USB Multilink and also the newer one; same result.

We also tried with CW 6.2 and same result too with the flash programmer.

Any hint on what to look next ?

Thanks in advance,

Robert

 

 

0 件の賞賛
返信
1 解決策
3,417件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Can you give me a little bit more details? 

 

this is with any project or only with a specific one?

 

regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,418件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Can you give me a little bit more details? 

 

this is with any project or only with a specific one?

 

regards

 

0 件の賞賛
返信
3,410件の閲覧回数
damorin
Contributor I

 

Hi, 

now it's working; it was two problems from two different sources (wrong CW version and a bug in the code).

Happy to say 'not a bug'.

 

0 件の賞賛
返信