2014 Freescale Cup Global Rules

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2014 Freescale Cup Global Rules

2014 Freescale Cup Global Rules

Official rules of the Global Freescale Cup!


New in 2014 - Roll-out of leagues:

Depending on region there will now be three leagues.  The Global race will only be stock league vehicles.

Stock League - Racing using approved components, less customization allowed

Custom League - Racing with less restrictions and custom hardware

Innovation League - More than just racing.  Complete an objective or task to score points and win.



Notes

  1. You can view this document in PDF format using the Action Menu bar.
  2. This rule set is for the Worldwide challenge.  Find your regional rules here
  3. The Worldwide challenge is only open to the stock (unmodified) challengers at this time.
  4. If you have ANY questions about these rules, post them in the comments section below.  If you have questions about regional rules, ask in your regional group.

Section 1: Team Requirements

  1. A regional championship team must run a “stock” (unmodified) league to qualify.
  2. Four person maximum team size.
  3. A team may have only one graduate student.
  4. Cars will be designed and constructed by students ONLY. 
  5. Participants, advisers, and audience are expected to exhibit good sportsmanship. Any inappropriate behavior or cheating may result in disqualification.

Section 2: Event Registration

  1. Entrants into the worldwide challenge are by invitation only. One invitation is extended to each regional champion team.
  2. One person from the regional champion team must register the entire team for the worldwide challenge within two weeks after the conclusion of the regional final. 

Section 3: Equipment Requirements

Each team shall use the same basic kit of parts as described below.  The following requirements are in place to keep the playing field level.  You must use one of the approved controller and motor driver boards.  If any standard component of the car model is damaged, then the same replacement component should be used.

Mechanical

  1. The original and unaltered equipment must be used in the entry. 
    • Outer tire treads and rim
    • Drive - DC motors
    • Transmission Ratio of Drive Motor
    • Servo Motor
  2. Allowed modifications and restrictions:
    • You may not change the wheel base (distance between wheels)
    • No part of the car shall exceed dimensions of 250mm/9.85in (W) x 400mm/15.75in (L)x 305mm/12in.(H)
    • You may drill holes and mount auxiliary pieces on the chassis assuming it is contained within the above dimensions.
    • You may change the orientation of the servo motor and related linkages.
    • You may add a "skin" to the car but it must be removable during inspection.
    • You may adjust or remove springs, linkages, and other non-essential pieces.
    • You may adhere the tread to the rim.

  Electrical

  1. Battery (purchase separately)
    • 7.2V, <=3000mAh, rechargeable NiCd or NiMH 
    • Only one (1) battery at a time may be used to power the vehicle and any attached hardware
  1. You must use one of the approved boards below to control your car.
    1. Control System
      1. FRDM- series of boards
        1. The FRDM-KL25Z is included but not mandatory to use.
      2. TRK- series
      3. Kinetis based TWR- series
    2. High Voltage Motor Control and Interface
      1. TFC-SHIELD
        1. The TFC-SHIELD is included but not mandatory to use.
      2. The Dual Motor Control Board from Landzo technologies.
  2. Allowed modifications and restrictions:
    1. One processor - No auxiliary processor or other programmable device is allowed. 
    2. The car must use a optical sensor to navigate
    3. DC-DC boost circuit may not exceed battery voltage.
    4. Total capacity of all capacitors should not exceed 2000 uF.
  3. Sensor Limits
    1. You may use additional cameras. 
    2. Maximum of sixteen (16) sensors
    3. Examples of sensor count: 
      • IR Transmitter/Receiver pair is 1 sensor
      • A CCD sensor is 1 sensor
      • The provided Line Scan Camera is 1 sensor
      • A hall effect sensor on two rear wheels is 2 sensors
      • An encoder mounted on one wheel is 1 sensor
      • A display (is allowed) does not count as a sensor

Section 4: Vehicle Inspection

Before the race, the judges will perform a technical inspection of all entries. This includes vehicle specifications, dimensions, and equipment requirements listed in Section 3.

  1. All cars must be placed in the Inspection area on or before the designated time.
  2. Once in the Inspection Area, you may not touch car until you are called to race!
  3. In the event of any violations, the organizing committee may disqualify the corresponding team.

Section 5: Timed Race Procedure

  1. Race order will be determined by a random drawing.
  2. When your team is called you may remove your car  from inspection area.  You will have two (2) minutes to prepare the car.
    1. Approved Adjustments - You may:
      • Configure parameters via on-board interfaces. (Switches, Knobs, etc.)
      • Alter the angle of your camera
      • Change batteries 
    2. Disallowed Adjustments -You may not:
      • Reprogram your processor
      • Configure parameters via wired or wireless communications.
  3. There shall be only one team member on the track at any given time. (excludes testing times)
  4. Before the 2 minute expires you must signal “Ready” to the referee before starting car.
  5. After the referee confirms “Ready”, the vehicle should leave the starting area within 30 seconds.
  6. Teams have THREE attempts to complete ONE lap.  The FIRST (not the best) completed time will be recorded.
    1. Example:
      • Attempt 1 – Vehicle goes to fast around a curve and goes off track.  Time is not recorded.
      • Attempt 2 – Vehicle makes it around track successfully.  Time is recorded.
      • Attempt 3 – Is forfeit because FIRST time (Attempt 2) has been recorded.
  1. After each attempt you have two minutes to make approved (see above) adjustments to vehicle.
  2. After the attempts, the team shall return the vehicle to inspection area.
  3. Event displays will post the times after each team races.

Section 6: Race Day Schedule

  1. Practice Time - Prior to final race, a test track will be available. Final calibration may be made at this time.  This will be organized with team slots and/or “free-time”.

  2. Reconfigure practice track to final track.

  1. Vehicle Inspection (see section 4)
  2. Timed Race
  3. Awards Ceremony

Section 7: Event Personnel

Organizing committee – A committee of senior judges and Freescale event organizers.  Will coordinate event day activities and mediate and resolve any disputes.

Referees -  Responsible for on-track activities. This includes race track management such as starting and stopping vehicles, as well as timing and scorekeeping. Comprise up of of faculty, student, and/or Freescale and industry employees.

Judges  - Interpret and enforce rule compliance.  This will be comprised of Freescale employees and members of contributing industry sponsors.

Event Personnel shall not aid any one specific team. Communication shall be open to all teams and shall not disclose any information that might compromise the fairness of the competition.

Section 8: Fouls, Failure and Disqualifications

The rules will be interpreted by Freescale and the organizing committee of the event.

            Foul, is a minor infraction, which results in time penalties.

Failure, results in the current attempt time not being recorded. Subsequent attempts are allowed.

Disqualification is a major infraction which results all times not being recorded.

  1. Referee will determine whether the racing car ran out of the race track and assign time penalties.
  2. Any of the following conditions will be considered a foul and will result in time penalty added:
    1. The race car fails to leave the starting area within 30 seconds after beginning of the race [+1 second].
    2. The race car fails to stop 2 meters/6 feet or leaves the track after crossing the finish line [+1 second].
  3. Any of the following conditions will be considered a failure and no time will be given:
    1. Three or more wheels leave the race surface.
    2. The racing team fails to get prepared for the attempt within the two (2) minutes allotment.
    3. The player touches the race car after the technical inspection without consent of the referee.
    4. The race car fails to finish within 120 seconds after leaving the starting area.
    5. Touching the car at any time between start and finish.
      1. "Start" - Once the vehicle crosses the starting line.
      2. "Finish" - Once the vehicle crosses the finish line.
  4. Any of the following conditions will be considered a disqualification:
    1.   Any off track equipment or behavior that may influence or impede cars.
    2.   Doing a Disallowed Modification anytime after Inspection.
    3. More than one team member in the playing field.
    4. Any cheating during the competition.
    5. Failure to pass the technical inspection.
    6. Equality and fairness will be ensured as much as possible on the condition of actual feasibility.  Disputes will be resolved by a vote of Freescale, members of the organizing committee, and judges.

Section 9: Timing/Scoring

  1. Time will be captured using an electronic gate and/or handheld timer.
  2. Time starts and ends when the first part of the racing car breaks the start/finish line.
  3. Fouls will result in the time addition to the car’s lap time.
  4. Disqualifications and Failures will result in no score.

Section 10: Parameters of the Racing Track

  1. A test track made from the same material as the final track will be made available on the day prior to the final race for calibration and design modifications.
  2. The actual layout of the final racing track will be unknown to competitors until competition day.
  3. Width of the racing track shall not be less than 600mm/23.65in.
  4. Material and dimensional specifications can be found on the community.
  5. Surface of the racing track is matte white, with a continuous black line (25mm/1in wide) on each edge of the track.
  6. The racing track can intersect with a crossing angle of 90°.
  7. The racing track can have inclines, declines,  and tunnels.

The rules and conditions are subject to change by Freescale if necessary. Freescale reserves the right in their sole discretion to cancel, suspend and/or modify The Freescale Cup race at any time. These official rules are drawn up in the English language. If these official rules are provided in any other language and there is a conflict in the text, the English language text shall prevail.

Freescale and the Freescale logo are trademarks or registered trademarks of Freescale Semiconductor, Inc. in the U.S. and other countries. All other product or service names are the property of their respective owners. © Freescale Semiconductor, Inc. 2014

Labels (1)
Tags (2)
Comments

Hi John, when will the next Global competition be organized?

Hi, I have some questions about these rules.

About the electrical restriction of section 3 "You must use one of the approved boards below to control your car.".
Q1: Are the rules talking about we cannot use homemade minimum system board (which is using kinetis MCUs, link) nor some homemade high voltage control board(link)?
---

About the line "One processor - No auxiliary processor or other programmable device is allowed.  "

Q2: Some sensors like camera, have build-in circuit which can do binarization in hardware( link), or camera with fifo chip ( link) .
Is the rule mentioned " other programmable device" includes these camera?
or is " programmable device" just meaning the kinds of MCUs or FPGAs device?

----
About "The Dual Motor Control Board from Landzo technologies."

Q3: Is the that this?

Thank you!

Deactivated user

John, have a look at those questions. Do you have a link for the dual motor control board from Landzo and can you confirm on the limitation of boards to be used?

Thanks

Hi Deactivated user I have a question, for the stocked league when it mentions "approved components" what does specifically mean? Does it mean that for the competition we can ONLY use the components listed in the “Mechanical” and “Electrical” sections? For example for the “High Voltage Motor Control and Interface” does it mean we can ONLY use one of the two boards mentioned (TFC-SHIELD and Dual Motor Control Board from Landzo technologies) or can we build our own board for the motor control stage?

Hi Jose Manuel, for the Worldwide Freescale Cup challenge, we are asking the students to use only the approved boards. You cannot develop your own custom boards. This is in the spirit of fairness and to avoid difficulties for the teams at the technical inspection in the case that their custom board is "hidden" or not accessible to verify that the board is conform to the rules (for example: no 2nd processing component or any other restricted component). Those rules are reviewed each year so stay tuned for any changes for the 2015 season.

Hi FlavioStiffan so just to be sure that means that in the competition we can NOT use a Motor Control board build by ourselves with analog components alongside a FRDM board, so in order to control the DC motors we are limited to use the two boards mentioned (TFC-SHIELD and Dual Motor Control Board from Landzo technologies) is this right?

Besides I have another question can we use small analog circuits build by ourselves? like for example an analog amplifier build with opamps or an analog comparator also build with opamps

Hi JoseManuelSandovalChavez I think the rules are pretty clear on what can be used. For the MCU and motor control part of the circuitry, only approved boards are allowed. In regards to the Small Analog amplifier, what is it related to? What's its function?

Ok thanks for the answer, in regards to the analog amplifier it will be used for conditioning of a signal coming from a sensor or a camera, the analog comparator that I mentioned will be used for the same purposes. For example we have a IR sensor that give a output voltage from 0 to 250 mV, we want to amplify the signal up to 3.3V or so, or want the comparator to only check if the sensor is in the white zone or the black line... thing like that.


Hi, it is ok to do signal conditioning. As long as you do not have another MCU part of it and that you control servos and motors via the authorized boards you are ok. Please make sure you are documenting your extra development with BOM (Bill of Material) and schematics in case there are any questions during the technical inspection.

Hi FlavioStiffan

Will there be tunnel for this year's Global Competition?

According to Competition Rules for Freescale Cup Malaysia 2014, tunnels will not be included in Global competition as well. Thanks.

The layout of the track is not known in advance so I cannot divulge to you if there will be a tunnel or not during the Worldwide Finals. Make sure your vehicle is within the measures authorized in the rules (height, width and length) so you are sure to fit into a tunnel if there will be one.

No ratings
Version history
Last update:
‎12-04-2013 11:26 AM
Updated by: