Which is the clock input pin of Vybrid?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which is the clock input pin of Vybrid?

Jump to solution
1,334 Views
george
Senior Contributor II

Hi all,

I wish to use an external oscillator without using crystal (24MHz and 32.768kHz).

In that case, are Clock signal inputs XTAL and XTAL32?

With a TWR board circuit diagram, EXTAL and EXTAL32 seem to be inputs.

(The direction of the arrow on a Vybrid symbol)

Best Regards,

George

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,160 Views
naoumgitnik
Senior Contributor V

Dear George,

Regards, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
2 Replies
1,161 Views
naoumgitnik
Senior Contributor V

Dear George,

Regards, Naoum Gitnik.

0 Kudos
Reply
1,160 Views
george
Senior Contributor II

Dear Naoum,

Thanks !!

It is my customer's question.

Probably, they also want to only know about 24MHz input.

Best Regards,

George

0 Kudos
Reply