Pin termination DDR address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin termination DDR address

ソリューションへジャンプ
1,909件の閲覧回数
keisukewatanabe
Contributor III

Dear support,

We are planning to use DDR with 14bit address input.

Please teach us how to terminate unused address bits of Vybrid (DDR_A[14] and DDR_A[15]).

In the reference circuit, unused address bit was connected to VTT_DDR3 via 47ohm resister.

Best regards,

Keisuke

ラベル(1)
0 件の賞賛
返信
1 解決策
1,745件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

You may use the same approach as the reference circuit does.

At the same time, termination is required for impedance matching of a toggling line, but unused lines do not toggle...

Best regards, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,746件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

You may use the same approach as the reference circuit does.

At the same time, termination is required for impedance matching of a toggling line, but unused lines do not toggle...

Best regards, Naoum Gitnik.

0 件の賞賛
返信