Which is the clock input pin of Vybrid?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which is the clock input pin of Vybrid?

跳至解决方案
1,340 次查看
george
Senior Contributor II

Hi all,

I wish to use an external oscillator without using crystal (24MHz and 32.768kHz).

In that case, are Clock signal inputs XTAL and XTAL32?

With a TWR board circuit diagram, EXTAL and EXTAL32 seem to be inputs.

(The direction of the arrow on a Vybrid symbol)

Best Regards,

George

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,166 次查看
naoumgitnik
Senior Contributor V

Dear George,

Regards, Naoum Gitnik.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,167 次查看
naoumgitnik
Senior Contributor V

Dear George,

Regards, Naoum Gitnik.

0 项奖励
回复
1,166 次查看
george
Senior Contributor II

Dear Naoum,

Thanks !!

It is my customer's question.

Probably, they also want to only know about 24MHz input.

Best Regards,

George

0 项奖励
回复